Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of [ H-5 ] Lgiht With Magnet Handle

[ H-5 ] Lgiht With Magnet Handle
Sales Price: 26.99 SGD
Review Rating: 3.60
5 Customer Reviews
5 star 2
4 star 1
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
If you drop screws etc. where hands do not fit into the gap
5
From Japan
On 2013-02-14 19:06:47
Feeling the hand reaches the itchy place! Bull - aluminum grip is good, the tip neodymium is strong and firmly picked up. This price is buying.
This review is about item#09202365.
Car hand light
3
From Japan
On 2013-01-11 14:56:05
Good
This review is about item#09202365.
Inspect the cavity with narrow entrance (φ 20) depth (about 180 mm).
1
From Japan
On 2012-11-09 15:25:49
The entrance was narrow (φ 20) I bought to see the cavity of the depth (about 180 mm) but the magnet was hard to insert at the entrance and the illuminance was weak. I think that there are some without magnets.
This review is about item#09202365.
Used for checking wiring, losing gaps, etc.
5
From Japan
On 2012-06-07 19:31:01
Audio equipment · PC etc. Peripheral equipment Used for looking things like gaps and gaps. The light is also brighter and easier to use than I thought. Until now confirming the clearance was using the bright one of the LED light, but the front one is hard to see with the reflection but with the magnetic pattern H5 with the flexible pattern can be confirmed by pinpoint and is convenient.
This review is about item#09202365.
For car maintenance
4
From Japan
On 2012-03-02 15:49:07
It is unavoidable because it is equipped with light, but it is difficult to use in a place where the tip is somewhat big and narrow, but it is good to use it for lighting in a recessed place.
This review is about item#09202365.
1
Customer Who Viewed This Item Also Viewed
Inspection Light,
Magnet Hand, Powerful Type
Magnet Hand
Magnetic Picking Tool
Magnetic Catch
Point Flash
Inspection Light
Searchlight
Check Light
(04491) F / Disk pad kit
SPOT LIGHT MINI
Inspect LED Light