Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Slide Rail S270

Slide Rail S270
Sales Price: 10.99 SGD
Review Rating: 4.00
6 Customer Reviews
5 star 4
4 star 0
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
For replacing slide rail for PC rack drawer
5
From Japan
On 2017-06-30 21:29:10
There is no play of the rail, the drawer feeling after exchange is very smooth and the sound is quiet.
This review is about item#9239273.
PC rack restoration
3
From Japan
On 2017-04-19 20:56:23
It is troublesome since it can not be installed unless it is fixed well when setting up. The movement was smooth It was used for repairing the PC rack but when considering from the price of the PC rack 2 thousand yen is high in the two things? However, it is hard to find because it is non-monotary except for monoterror, so I just thought that it would be different even if the wall thickness of the rail members was different, but perhaps the same level of normal strength.
This review is about item#9239273.
To withdraw construction work furniture
1
From Japan
On 2017-02-13 10:59:42
Because there is no statement that desorption is impossible, it was not possible to install on the side where the driver does not enter or the narrow place. Although there was a statement that desorption is impossible for other goods, it was not in this item of goods.
This review is about item#9239307.
OA disk rail
5
From Japan
On 2013-04-02 13:41:01
Work was also easy to install with dimensions as stated.
This review is about item#09239282.
I used it to make a drawer cupboard in a special place in the kitchen
5
From Japan
On 2013-01-25 17:14:24
· Since the maximum depth of the mounting dimensions was 250 mm, we searched for those on the market but there was nothing less than 300 mm · As a result of investigating various things on the net, we purchased adaptation items at your company · I think that it may be useless because it may be less demand as it is a special product, but it was a pity that it was long until delivery
This review is about item#09239255.
For replacing the slide rail of the damaged PC rack sliding table
5
From Japan
On 2011-05-22 13:07:04
It took a bit of time to arrive, but compared to the slide rails originally installed in the PC rack, I felt that the quality and strength were much better.
This review is about item#09239291.
1
Customer Who Viewed This Item Also Viewed
European Slide Rails
Slide Rail 17 New Series
Slide Rail ND150
Double Step Slide Rails
Slide Rail ND160
Slide Rail
Center Slide Rail
Slide Rail S101
Three-step Slide Rail
Accuride: Slide Rail
Slide rail