Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Gas Spring Y2 Series

Gas Spring Y2 Series
Sales Price: 45.09 SGD
Review Rating: 4.86
21 Customer Reviews
5 star 20
4 star 0
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 20 of 21 Reviews .
Britain old car of the damper for opening and closing the hood
5
From Japan
On 2016-06-27 21:10:57
Replace also easy to have an effect as expected.
This review is about item#09229577.
Component replacement
5
From Japan
On 2016-02-29 16:23:46
Suddenly condition becomes worse, order Reach the next day, was saved. Because the price was cheaper than to order the trader, it is satisfaction.
This review is about item#09229595.
As an old car of the rear glass hatch of the damper
5
From Japan
On 2015-04-05 20:09:00
Old car gas spring supported the glass hatch had thought the exchange have I Heta. In but was looking for a genuine parts Sure enough Out of print, was selected order things here looking for those close to the size exchange. Enough to use it is now pleased to understand. It will surely repeat. It is satisfaction.
This review is about item#09229604.
For skylight
5
From Japan
On 2014-09-01 10:14:38
Little processing at the mounting bracket was necessary, but it is working well. It was expected replacement of the two, but it is enough to operate a single exchange. One Is it possible I would like to return because I bought two? It is expensive thing because the idea to leave this is I feel too good. Thank you if possible if.
This review is about item#36291001.
Soundproof cover
5
From Japan
On 2014-07-08 17:08:17
Packaging, quality is also good, it was perfect.
This review is about item#36290992.
Loading platform bodywork
5
From Japan
On 2014-05-30 15:03:37
Very, we are satisfied.
This review is about item#09229543.
Parts replacement of Hawk lift
5
From Japan
On 2014-04-10 22:31:36
Products a strong, there is a sense of security, likely to be used long, very satisfied.
This review is about item#00270122.
At the time of vehicle inspection
5
From Japan
On 2014-02-01 04:47:27
Cheap is good
This review is about item#09229586.
Use the retractable hood of the truck holding company
5
From Japan
On 2013-11-22 23:00:02
Hood is no longer able to self-opening and closing from the gas spring that had been attached to a retractable hood of the truck, which was purchased secondhand leaking oil. Repair it was cheap is better to buy in Monotarou than the order at the factory. Thanks, hood We are also very pleased to return to the normal state.
This review is about item#09229577.
Used to head weight reduction for the balance of the machine tool
5
From Japan
On 2013-10-29 13:36:26
Y2102 and 2088 by adding the purchase because it was remodeled not it this time machine to use for head balance from 10 years ago has been used in three. When you remove the Y2102 I tried to put weight but I was relieved because it does not budge.
This review is about item#09229543.
Haikemurimado
5
From Japan
On 2013-10-10 14:51:40
No particular problems
This review is about item#36291017.
Door of the dishwasher
5
From Japan
On 2013-08-26 19:23:52
It was gas spring replacement of the door of the dishwasher. It can be mounted immediately. The skilled in the estimate was 50,000 yen in two. It is very satisfactory.
This review is about item#09229647.
Used as a trunk of the shock of the Lotus Esprit
5
From Japan
On 2013-06-24 20:32:07
Very cheap and can also be used in a heavy trunk, repair was able, should be noted, it was able to be mounted without almost processing
This review is about item#09229622.
Their bus rear trunk replacement part
5
From Japan
On 2013-06-01 21:28:02
Exchange for flip-up trunk of the gas spring is stood to. Very condition is good ♪
This review is about item#09229543.
Use the flip-up gate of the garage
5
From Japan
On 2013-05-25 23:17:12
Each place has very pleased dimensions fit perfectly with the old gas spring because there was a complete drawings of dimensions. Operating after mounting is no particular problem.
This review is about item#36291026.
Repair work
5
From Japan
On 2013-05-18 20:55:53
I was able to purchase smoothly. Delivery time also arrived ahead of schedule. Opportunity is there is I would like us also to use.
This review is about item#36290992.
It is using the absorber of the rear gate of the old car.
5
From Japan
On 2013-02-15 15:28:47
Rear gate damper and size-stroke primary civic was the Pittashi. Can be replaced for a Pong with, genuine parts manufacturers was very helpful because it was lack of state.
This review is about item#36291026.
Built-in to the machine tool
5
From Japan
On 2012-05-01 00:50:33
Better to choose the size and pressure Durability does not know because you just use
This review is about item#09229631.
In the rear of the truck, which was purchased in the Middle Ages there is a door of feather-up type, used as an alternative to part of the "Y3006" of the support.
5
From Japan
On 2012-03-26 15:09:10
There is a door of feather-up type in the rear of the truck, which was purchased in the Middle Ages, where the "Y3006" of existing component is to arrange replacement parts and trying to repair since become head down when the door is opened by the aging, 60 this There is a manufacturer replied that not ship only in units, tentative plan as a result, the product length and running stroke length, and it is determined that it would be possible alternative in the "Y2157" exchange from such as gas pressure, and it is operating without current problem .
This review is about item#36291026.
Used for the opening and closing of the cover
2
From Japan
On 2010-05-27 23:00:23
We want to lengthen a little more life
This review is about item#09229586.
1 2
Customer Who Viewed This Item Also Viewed
Gas Springs
Gas Spring Y0 Series
Gas Spring Y3 Series
Gas Springs
Gas Spring KSF-Series
Gas Damper
Bracket
Gas Springs
KNURLED KNOBS
Gas Springs
Gas Springs
Mounting Bracket