Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Fingerstall For Industry

Fingerstall For Industry
Sales Price: 22.99 SGD
Review Rating: 3.00
5 Customer Reviews
5 star 0
4 star 2
3 star 2
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Frp processing
3
From Japan
On 2017-04-05 16:51:14
In frp processing, when bubbles collapse and touch-up work when the resin is semi-hardened gel state are often used as fingers, it is unnecessary to put gloves again when only the index finger is used, and bare hands are made of resin It is troublesome to get on and sebum on the application surface is also a little concerned. I tried buying it by saying. Although I feel that my fingers are thick and ring finger size is about 21 in index fingers, I feel it is too tight, but I do not have to use it for a long time and I just throw it away for a few minutes so there is no problem, but for a thumb of about 23 Although it is a few minutes even a few minutes, the blood of the finger changes. It is hard to say that the tight one is preferable for my purpose, but if you think about using for more than an hour etc, people should be careful who uses L of rubber gloves. For atmosphere, it is close to the thickness of index finger about the size of m and s of disposable rubber gloves, but, if it is a thin female female, it may be unrelenting. I think that it is a good size for men.
This review is about item#9242021.
Hydraulic work
1
From Japan
On 2015-03-02 18:16:48
Hand size is M size with gloves and fingers are not thick. When I tried using this finger cot, it was impossible to continue to use with the finger becoming discolored with strong tightening feeling for about 5 minutes.
This review is about item#09242021.
Adhesion
4
From Japan
On 2012-12-12 18:33:31
I used it to spread the bond on the adhesive surface. Somehow it went well.
This review is about item#09242021.
easy work
3
From Japan
On 2012-06-14 12:51:59
It is fairly thin compared to general office work, so it may be easy to break depending on work. Ideal for prevention of dirt on the fingertip and slip prevention. Since it is rolled, it does not take up space and it is easy to fit. Because it is a consumable item, it is saved because it is cheap.
This review is about item#09242021.
For cleaning and maintenance of the machine, use it inside the gloves
4
From Japan
On 2012-02-21 14:00:22
It seems to be habit, I think that it will be useful because fingers can prevent it from oil soiling
This review is about item#09242021.
1
Customer Who Viewed This Item Also Viewed
Antistatic Latex Finger Cots
Finger Cot
SPORE Finger Cot
Finger Stall
Spore Brim Finger Stall
Spore Brim Finger Cots Powder Tri
Fingerstall for Pearl Industry
Green Knoll Finger Sacks
Nitrile made finger sack Serekotto
NR work cot (OFF)
Nitrile made finger sack Kyuanosu
NR work Cotto cut wound