Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Aluminum Board Roll, Adhesive

Aluminum Board Roll, Adhesive
Sales Price: 22.99 SGD
Review Rating: 1.75
4 Customer Reviews
5 star 0
4 star 0
3 star 0
2 star 3
1 star 1
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Bathroom Wall
From Japan
On 2017-02-10 00:37:17
It is hard to be flat with the thickness, difficult to adhere to the wall, difficult to use
This review is about item#9242213.
Aluminum door repair
From Japan
On 2016-11-14 19:11:38
I think that the product itself is probably not bad, but it is unused. The reason was that I could not use it because there was a difference between the feeling I saw on the screen and the real one. The item was too good for shiny gloss and it did not match with the real thing. The judgment on the screen is difficult.
This review is about item#9242213.
Heat reflection
From Japan
On 2014-12-19 15:17:29
Insufficient performance of adhesive material. The curling tends to remain strongly, and when it comes in contact with moisture it expands and softens and peels off. Outdoor use is impossible, even if it is used indoors, the same result due to the situation of pasting object and condensation.
This review is about item#09242204.
Used on the wall of the sink side
From Japan
On 2013-11-15 14:29:26
Adhesion is weak and aluminum itself is also hard and it is hard to remove curling.
This review is about item#09242204.
Customer Who Viewed This Item Also Viewed
Aluminum Board Roll
Stainless Steel Board
Aluminum Sheet
Round OA chair
Stainless steel sheet
Aluminum Sheet Plate