Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Flag Hinge With Stainless Surface

Flag Hinge With Stainless Surface
Sales Price: 13.99 SGD
Review Rating: 4.75
4 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Replace the aluminum sash
4
From Japan
On 2018-02-22 16:08:40
Although this was the only one that fits the existing hinge, the position of the hole did not match slightly with the old type, but there is no problem as product performance at all.
This review is about item#9359506.
Karaoke Box Store Single Room Used as a door hinge
5
From Japan
On 2015-05-01 23:38:01
I think very well as an easy-to-use and inexpensive product.
This review is about item#09359427.
Used to replace defective hinge
5
From Japan
On 2014-03-12 23:43:48
It is good that you could install without having to worry too much when installing on the left and right. It is recommended that you have prompt response as stock can be installed without regard to left and right selfishness.
This review is about item#09359427.
Machine equipment maintenance work
5
From Japan
On 2013-04-17 08:29:48
It was a recommendation point that right and left (L · F) was displayed on the hinge. Even when purchasing next time it is easy to understand. I'm happy if I can purchase it a little cheaper if possible.
This review is about item#09359323.
1
Customer Who Viewed This Item Also Viewed
Flag Hinges
Lift Off Hinge
Flag Hinge
Stainless-Steel Flag Hinge
Stainless Flag Hinges
Stainless Steel Hinge
Stainless Flag Hinge
Hatahinotoban
Hatahinotoban (both left)