Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of DX Oil Bristle

DX Oil Bristle
Sales Price: 2.99 SGD
Review Rating: 4.50
10 Customer Reviews
5 star 5
4 star 5
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Paint painting
4
From Japan
On 2018-03-11 15:39:52
I want a soft brush made of nylon with this hand brush, this part can be ordinarily used but it is too good to cling to the hair, it is difficult to go out with paint, even if made from nylon too painfully paint when the pain is over at the end of painting The clothes become dirty, a small small type brush of a small size, I want a soft brush made of thin nylon with a length of 35 to 40 cm of hair and a width of 20 to 30 cm, this brush is not bad, but ,
This review is about item#76235537.
For painting
5
From Japan
On 2017-08-17 08:25:24
I used it when painting the bicycle frame. It's a nice item.
This review is about item#76235537.
Painting, touch up
4
From Japan
On 2017-06-09 09:10:47
Is good! It is easy to use. I would like to thank you if the price cheaper a little more!
This review is about item#09514696.
Application of oil paint
5
From Japan
On 2017-05-12 16:33:53
For the first time I bought a brush for oil paint, but it is reasonably priced cheaply and disposable is also reasonable.
This review is about item#76235537.
Iron part paint
5
From Japan
On 2016-06-22 02:50:00
I am using 20 mm. Both inclusion and exhalation are satisfactory. Although oily brush is disposable, it has not been better to be inexpensive, but the quality is proportional to the price and rarely satisfies cheap items. Now, with this, I am in trouble because there is no brush point where I bought a lot before. Not limited to this, it is recommended to wash the brush before use (dry in case of oiliness). Also reducing hair loss improves usability and finish.
This review is about item#76235537.
When painting work
5
From Japan
On 2015-11-16 08:36:35
I am using it without problems.
This review is about item#09514687.
Building painting
4
From Japan
On 2014-11-08 13:43:30
Including and waist is good. It is quite good for price.
This review is about item#09514671.
Painting to the steel surface (touch-up etc.)
4
From Japan
On 2014-07-30 14:03:01
Hair is also repetitively done without falling out
This review is about item#09514696.
Mainly painted iron rails and stairs
4
From Japan
On 2012-12-03 14:51:53
Hair elasticity is good. The inclusion of paint is also good. However, if you reuse it will result in more hair loss, so if you consider the price, is it disposable?
This review is about item#09514671.
Painting
5
From Japan
On 2012-07-26 21:58:17
The hair is soft and easy to use. I think that it is a brush suitable for painting of oil paint.
This review is about item#09514687.
1
Customer Who Viewed This Item Also Viewed
Oil Based Paint Brush,
Stick Angle Paintbrush
Brush
For DX Water
Steel & Bridge Brush
Brush for Painting Wave
Brush for Extra Oil Bases
Absolute Brush
Varnish Brush,
SUS NUT COVER 58L 41mm 6/pac
Multi Purpose Brush
Refill Rollers, Small
Multi Purpose Brush