Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of New Years Event Board For Horizontal Writing

New Years Event Board For Horizontal Writing
Sales Price: -
Review Rating: 4.64
11 Customer Reviews
5 star 7
4 star 4
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Office sales schedule
5
From Japan
On 2015-06-30 17:04:58
For sharing three people, I draw a line with an oil pen and use it in three divisions. Quality is good for the price, I like it very much. The accessory pen is unexpectedly easy to use. Eraser is not good, but it is not like I have to replace it immediately. Please note that wall mounting screws and nails are not included.
This review is about item#09528881.
Private use
5
From Japan
On 2015-05-20 14:37:20
It is a good prize with good size and quality, excellent cost performance.
This review is about item#09528881.
Fill in work / event
4
From Japan
On 2014-06-13 14:05:02
The size is also good, so it's easy to use.
This review is about item#09528872.
We will do it in just the right size to fill out the construction schedule.
5
From Japan
On 2012-11-27 23:41:04
It is easier to write than I thought it is refreshed even if it is attached to the wall so I am also proceeding to those of the same company.
This review is about item#09528881.
Work schedule
4
From Japan
On 2012-09-28 15:21:46
It was cheap, but there was a dent on the board.
This review is about item#09528881.
schedule
5
From Japan
On 2012-04-13 18:24:38
Amount is cheap Can use more than I thought
This review is about item#09528881.
Used as work schedule
5
From Japan
On 2012-04-05 17:27:14
The sliding mechanism of the hanger bracket is very convenient and easy to adjust the mounting location. This price is cheap and it can be used without any inferiority to those made by manufacturers. The difficulty is that erasers (letter erase) are cheap and difficult to use. The attached magnets are too small to be really okay. These two points are complaints if they become cheaper as an option.
This review is about item#09528872.
I am writing a timetable for a month's work.
5
From Japan
On 2011-11-26 11:19:16
It is a good feeling that the width is just as easy to write clearly and clearly expressible letters.
This review is about item#09528881.
As a light work schedule at the office.
4
From Japan
On 2011-05-19 17:40:14
It would be great if pen placement disappeared. But I also want a pen placement. Because it protrudes out of the way.
This review is about item#09528872.
It is big and easy to see
5
From Japan
On 2011-04-20 18:19:55
Easy to use
This review is about item#09528881.
For describing the work schedule at the entrance of the office
4
From Japan
On 2010-02-22 17:31:06
It is very easy to install and reattach the hanger bracket by sliding it. I would like to make improvements If you set it in the wind blowing entrance, it is flawed by the wind and it flies, so I think whether there is a hook metal fitting that can be fixed to the bottom or side. Also, since the resin parts of the corner are easy to break, I think whether resistant resin or rubber material is good. Or if you are a metal part I think that texture will be better as well.
This review is about item#09528872.
1