Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Folding Cross Wrench

Folding Cross Wrench
Sales Price: -
Review Rating: 3.00
5 Customer Reviews
5 star 2
4 star 0
3 star 1
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Tire change
3
From Japan
On 2016-07-01 16:10:32
I am using only a little yet, since I can fold it, I feel good without taking the place to mount on the car. Afterwards if I do not have any trouble such as disengaging buttons for everyone's review?
Tire exchange
1
From Japan
On 2016-02-15 18:12:55
With the exchange of the second tire, the push button flew away. It is a defective product.
This review is about item#09600071.
Tire exchange
1
From Japan
On 2015-03-23 13:45:59
I took off the button after I used it twice. I want to be replaced as it is defective.
This review is about item#09600071.
Tire exchange
5
From Japan
On 2014-04-11 16:02:48
It is cheap, it is convenient to use a box.
This review is about item#09600071.
We can also use other than tire exchange · · · minivan!
5
From Japan
On 2013-11-19 21:33:23
I used Emerson's folding cross wrench but broke the socket part and purchased alternatively. It is securely fixed only by operating the lock part in the middle. Usability is also better than Emerson. Because the socket part is also thin, I think that it will enter if it is not so foil. One of the cloths is made to be able to use a 12.7 mm box socket and it is supreme. Lock Nut Box etc. The size you can use can be used not only for exchanging tires but also for use!
This review is about item#09600071.
1
Customer Who Viewed This Item Also Viewed
Cross Wrench
Cross Wrench
cross rim wrench
Cross Wrench
European Lug Wrench
Folding Lug Wrench
Cross Wrench
Cross wrench
Cross wrench (aluminum wheel correspondence)
Cross slim wrench
Cross Wrench, Aluminium Wheel Supported
12.7sq. Lug Wrench
Caliper Clamp Screw
Double Power Cross wrench
Lug Wrench