Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Wheel, Rubber One Wheel425 E-R

Wheel, Rubber One Wheel425 E-R
Sales Price: 2.99 SGD
Review Rating: 4.63
27 Customer Reviews
5 star 22
4 star 2
3 star 2
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 20 of 27 Reviews
The wheels of the dolly which had been stored for a long time deteriorated and the rubber peeled off and it became useless and purchased for replacement
5
From Japan
On 2018-04-13 14:44:25
I purchased watching only the wheel size and pin pitch, but the wheel exchange went well with accurate notation and revival as new! It was saved very much when I found it in a monotalou where I gave up parts without even knowing the manufacturer. I will also use it.
This review is about item#6707617.
Wheel exchange of L type cart
4
From Japan
On 2018-04-10 18:16:46
Since it was attached from the beginning, because the wheel was poor, I changed it for this item because it was deformed. Because the wheel shaft diameter was the same, it was easy to replace, the nylon bearing also slipped well, it was smoothly rotated, but the weight is quite heavy, the rubber is stiff, so load bearing is likely to be, but the vibration absorptivity is low I think.
This review is about item#35772134.
Machine in the factory
1
From Japan
On 2017-12-20 16:59:27
I bought it with the same model number but the inside diameter was different. I neglected to check the dimensions.
This review is about item#6619785.
Wheel of elastic gate
5
From Japan
On 2017-11-04 11:40:36
Difficult to open due to wheel wear with quick delivery soon cured.
This review is about item#35772125.
toolbox
5
From Japan
On 2017-09-19 15:40:33
I was looking for screw-in type casters as well as wheels I endured it without size (pitch).
This review is about item#6707617.
Restaurant Wagon Casters
5
From Japan
On 2017-09-18 16:40:13
Smooth movement, quiet and great! ! Next time thanking you ^ ^
This review is about item#6619785.
Repair of bike lift
5
From Japan
On 2017-08-19 20:30:14
After all the new article, the movement is smooth and the lift-up became easier.
This review is about item#35675936.
Repair of carry bag
5
From Japan
On 2017-05-17 18:38:06
Size is perfect, you can easily purchase without making mistakes.
This review is about item#35675936.
For replacing the suitcase
5
From Japan
On 2017-01-18 15:27:27
The type and size are large and the price was affordable and easy to ask and was very good.
This review is about item#35772125.
To exchange casters
5
From Japan
On 2016-12-01 22:50:06
I'm using a pro box suitcase, but the castors collapsed and exchanged the same product.
This review is about item#35772125.
Suitcase caster substitution
4
From Japan
On 2016-08-28 12:14:34
Less wear and durable and less breakage
This review is about item#35675936.
Changing broken wheels in dolly
5
From Japan
On 2016-07-21 08:38:50
As the truck that got rattled as rubber got rattled replaced it, it began to move smoothly. Was saved.
This review is about item#06707617.
For dolly wheel replacement
5
From Japan
On 2016-03-10 21:57:52
It was just right size. In the case with fittings, we decided to replace only the wheels because the mounting holes do not fit.
This review is about item#06707617.
Suitcase caster repair
5
From Japan
On 2016-01-17 19:43:52
It was good at best matching
This review is about item#35772134.
It is a good item.
5
From Japan
On 2015-11-02 18:35:16
We ordered only the tires of the casters here unusually. Moreover, the tire size 42 mm is even less. Hopefully, the size on this is 50 mm, but I actually want a tire of 45 mm but I do not seem to handle it in Monotaro san. I would like you to have a 45 mm size tire ready.
This review is about item#06619785.
Racing cart stand tire
3
From Japan
On 2015-09-01 00:51:30
I thought that I would roll more as I replaced the tires, but it was normal. The tire with the bearing may be better. . .
This review is about item#35772125.
Exchange of wheels of dolly
5
From Japan
On 2015-08-24 18:29:40
The dolly being used has come to produce vibration, loud noise and vibration due to the deterioration of the wheel. As a result, we were considering disposal of dolly, we found this product and purchased it and tried repairing it. As a result, the trolley became to move smoothly so as to make a mistake, and it became very comfortable. I was impressed. This is the only one.
This review is about item#35772134.
Component replacement
5
From Japan
On 2015-02-14 13:19:42
For parts replacement, we are pleased with purchasing parts by itself. Since things are hammer, there was no worry.
This review is about item#35772125.
Wheel change of dolly
3
From Japan
On 2015-02-06 10:56:11
I can use it smoothly after replacement.
This review is about item#06707617.
Wheel change of dolly
5
From Japan
On 2014-11-04 10:50:30
It is used for exchanging the wheel attached to the dolly. Hammer caster is high quality, so I trust it. It is saved because the wheel itself is not readily sold to the home center.
This review is about item#06707617.
1 2
Customer Who Viewed This Item Also Viewed
Wheel, Rubber Wheel
Wheel, Rubber
Wheel, Rubber Wheel425 S-R
Wheel, Rubber Wheel425G, E, S-R
Wheels, Urethane Cars439 G-Ur
Wheel, Rubber Wheel427S-Rd
Wheel, Rubber Wheel445 G-R
Wheel, Hard Rubber Wheel
Wheel, Urethane Wheel439E-Ur