Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Washing Bottle, Bs Type

Washing Bottle, Bs Type
Sales Price: 2.99 SGD
Review Rating: 4.71
14 Customer Reviews
5 star 11
4 star 2
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 14 of 14 Reviews
For mission and differential oil exchange
4
From Japan
On 2018-01-23 13:55:13
It seems to be in good shape on feeling that I tried but did not receive the essential oil. We will review again if we make a mistake in implementation.
This review is about item#10070313.
It is useful for lubricating the sewing machine
5
From Japan
On 2017-11-11 12:00:44
It is OK to reach the place where the crane head is long and narrow. It is a feeling that the hand reaches exactly itchy places. It was good to be found with a length that is not on other sites.
This review is about item#10070286.
Water supply to a tank etc.
4
From Japan
On 2017-09-03 23:35:15
I think that it can be used for watering in aquariums, watering for planting trees, other things, and the price is also cheap.
This review is about item#10070286.
Machine maintenance
5
From Japan
On 2017-08-05 18:14:39
I wash parts and put some water to wash the parts. In addition to temperature and humidity calibration, use it with fountain solution etc. I like it because it is also hard to deteriorate. Compared with other companies it got degraded and water leaks etc. are early but this product is still not leaking water. I also want to purchase.
This review is about item#10070304.
When subdividing and making sample of lotion
5
From Japan
On 2017-01-12 22:41:27
When subdividing it, it was good to be injected and it was good to be used very well.
This review is about item#10070286.
Water change of fish bowl of Medaka
5
From Japan
On 2016-12-16 21:07:15
Purchased for water exchange of fish fish bowl of Medaka. Was it a bit small? I am satisfied with the performance.
This review is about item#10070295.
When solving a rock paint
5
From Japan
On 2015-12-14 14:36:23
The bottle is supple and easy to use. The tip of the pipe is fine and it is possible to subtle water subtly.
This review is about item#10070304.
For manometer's water replenishment
3
From Japan
On 2015-12-11 14:47:19
I thought that it was easy to do because the point was sharp, but after all it entered the air did not go well. I think that there is no choice because its usage is different.
This review is about item#10070295.
Lubricating details
5
From Japan
On 2015-09-02 00:10:21
I used it for lubricating details because the mouth ends well in small places, and it is useful.
This review is about item#10070286.
I use it in the drilling work,
5
From Japan
On 2013-10-23 15:34:32
In the steel plate drilling work, it is possible to precisely adjust the amount of cutting oil to the desired location, and the tip of the nozzle that can produce the desired amount is as close to the needle hole, so adjustment of the liquid amount is very useful because it can be freely adjusted by the grasping strength. I like the fact that there is no unnecessary discharge by the outside air temperature by adjusting the nozzle up and down. I really recommend this usage.
This review is about item#10070286.
Water injection into the measuring cylinder than washing
5
From Japan
On 2013-03-23 17:47:17
Because the body is so soft it is hard to get tired. However, because the diameter of the nozzle screw is small, water injection may be difficult. It depends on the environment.
This review is about item#10070304.
Replacement of brake fluid
5
From Japan
On 2012-05-21 15:08:18
I used it to extract the old fluid and to replenish the new fluid. It was easy to work because the nozzle was slender. It is convenient to have one.
This review is about item#10070304.
Blowing kerosene
5
From Japan
On 2011-11-21 22:31:38
It is cheap and durable, it is also nice to say as one.
This review is about item#10070304.
Cleaning the engine etc. by putting kerosene
5
From Japan
On 2009-05-30 14:42:40
As the grip part is treated with satin finish, it is OK to slip hard. There is no leakage from the tube and cap part at present.
This review is about item#10070304.
1
Customer Who Viewed This Item Also Viewed
Wash Bottle
Gas Venting Wash Bottle
Washing Bottle
It Is Soft Washing Bottle
Wash Bottle
Round Wash Bottles
Polyethylene Washing Bottle
PFA Wide Mouth Wash Bottle
B-Type Detergent Bottle
Color Cap Narrow Mouth Wash Bottle
Fine Washing Bottle Thin Mouth