Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Work Belt Long

Work Belt Long
Sales Price: 14.99 SGD
Review Rating: 4.17
6 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Used for everyday use
4
From Japan
On 2018-01-15 15:35:02
There is no problem for use as it is long. However, please be aware that it will take some time to use and become familiar to some extent because it is rather hard.
This review is about item#10078607.
For when going out while working
5
From Japan
On 2017-10-08 01:48:12
In consideration of scratches on work targets, I do not wear a belt and I put on shirts and wear working trousers, but when I go out or going to school for children, the number of times I go to school is high, and even though I am working clothes I need to wear a belt, so I decided to buy a belt this time, but I think that this is good. It is fairly large, and since it is the center area of ​​the belt hole because it does not cut in 46 to 48 inches in inches, there is a length that can cover up to 50 inches longest pants. Although it is a metal fitting, not only there is a loop of metal in the buckle area, but also around 10 centimeters there is a loop metal fitting, so you can easily remove it if you get in the way. The hardness is also firm, it is hard to become like a belt that is curved and curled at the center of the waist side, which is often found on a soft belt. It is not in an environment to sweat so much that the belt gets wet, but it will be dryer than the skin and cotton belt earlier, it is sanitary and dirt-resistant. It is not suitable for those who do not like hard belts, but you can recommend it to those who think they want something cool.
This review is about item#10078607.
Working wear
5
From Japan
On 2016-04-18 22:00:34
It is very nice for fat people.
This review is about item#75173603.
Electrical installation work
2
From Japan
On 2015-10-13 08:54:22
Although the strength of the belt itself is quite strong, it feels strong and firm, but there is no belt threading in the buckle and instead of a resin made thing is attached but it seems to fall out and be lost when not in use.
This review is about item#10078616.
Everyday use
5
From Japan
On 2015-04-05 23:31:17
Even with a belt of a size of 130 cm and a long size with a weight close to 100 kg, this size can be purchased securely as this size is comfortable at the time of purchase. When you tighten the belt, the hard weave 4 cm width also makes you feel better.
This review is about item#10078607.
Wear on work clothes
4
From Japan
On 2014-05-17 18:23:46
It is quite durable and long size is very pleased with this price. Since the position can be fixed with a hole, it does not loosen and the shirt has come off. However, it is a disadvantage that getting caught for a while when passing through the loop at the time of wearing.
This review is about item#75173603.
1
Customer Who Viewed This Item Also Viewed
Work Belt
Working belt 1 pin 5 layers
Work Belt No.1002
Working Belt King Size
Work Belt
40mm Work Belt
Nylon Ip Belt 38
PP 1 Pin Belt
Web Work Belt
Working belt 2 pin
Denim short-sleeved shirt 87504
Nylon Belt
Casual Belt