Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Sliding Latch

Sliding Latch
Sales Price: 67.99 SGD
Review Rating: 4.75
4 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Ceiling embedded ventilation fan, air conditioner installation, electrical construction, antenna construction etc.
5
From Japan
On 2015-03-30 23:05:48
It is good that work can be done quickly,
This review is about item#10080113.
Bolt fixing · Similar work as that
5
From Japan
On 2010-02-18 15:16:39
I do not have any dissatisfaction with using it, but can not you add 17 sockets at the price of 1,000 yen increment? Adding a socket of 17 or 19 ... I used the same type of ratchet of aluminum before, but the aluminum weakly deformed in about 3 years ... I returned to this ratchet with weight . Considering the endurance years it is here.
This review is about item#10080113.
Rack and other bolt tightening
5
From Japan
On 2009-07-15 02:11:15
There is a hole in the center for attaching a fall prevention tool, so I want you to attach a ring or something in advance. I'd like you to handle Negros' 17 mm socket as a set.
This review is about item#10080113.
Since the nut size such as wiring rack and piping installation is different, it is best for tightening.
4
From Japan
On 2008-12-14 15:56:01
It is good that you do not have to have many fastening tools, because it is long, it is good to be able to use it in a certain narrow section. Can we make the material lighter?
This review is about item#10080113.
1
Customer Who Viewed This Item Also Viewed
Slide Latch
Ratchet Glasses Wrench
Both slide latch
Board Ratcheting Wrench
4 size Plate Ratchet Wrench, Long Type
4-in-1 Plate Ratchet
Ratchet Offset Wrench
8 Way Wrench
6 function multi wrench
RAKULATCH with 17mm SOCKET