Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of All-Purpose Scissors, powerful type

All-Purpose Scissors, powerful type
Sales Price: 69.99 SGD
Review Rating: 3.00
6 Customer Reviews
5 star 1
4 star 2
3 star 1
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Used as a waist tool for electrical work.
3
From Japan
On 2015-10-11 13:15:49
Both single bar and double bar can be cut well, but it is difficult to exceed the width of the blade.
This review is about item#10097911.
Cutting of brass and stainless steel
1
From Japan
On 2015-01-04 12:09:48
Materials exceeding the width of the blade are very difficult to cut. Also, when cutting 0.8 t of SUS 304, the blade spilled. A product that only laughs (laugh)
This review is about item#10097911.
Cut 0.8 piece of iron plate
1
From Japan
On 2014-08-16 23:19:26
There is no escape of the iron plate, only the width of the scissors can cut. I bought it and failed. Larger steel materials of larger thickness are not suitable.
This review is about item#10097911.
Cutting of light roof material
4
From Japan
On 2013-06-24 19:20:37
I think that cutting ability is not a problem, but I thought that if the opening of the handle is a little more, it will be easier to work with one hand.
This review is about item#10097911.
Ceiling opening etc.
5
From Japan
On 2013-03-28 14:47:50
Lightweight Used to cut the ceiling substrate. Although the sharpness is outstanding, since the opening is small, the M bar can not be cut at once, but it does not become difficult because it does not apply force because it is a multiplier force
This review is about item#10097911.
Cutting of 1 mm thick SUS 304 plate
4
From Japan
On 2012-10-14 16:39:57
We cut 1 mm thick SUS 304 with a cheap bin force shears up to 0.6 mm stainless steel, but we introduced this product with boost capability that can cut up to 1 mm because it is too tiresome. As work, there was improvement to a degree, which makes it a bit easier than before. However, I think that it is considerably bare ability to stainless steel 1 mm. It is easy to cut by boosting structure, but it is painful for people with small hands, because you can not fully utilize the blade unless you open the handle gently. Since there is no function to cut without lifting the board, basically there is only a cutting ability enough to cut with a straight line of one cut. I think that there is no one who does not notice, but the U-shaped board in the example of use is cutting it with a V-shaped slit in it and it is not cutting the folded part as it is.
This review is about item#10097911.
1
Customer Who Viewed This Item Also Viewed
Metal Cutting Shears
Band Cutter
Metal Cutting Scissors
Cutter,
Long Scissors
All Purpose Shears
Scissors
Tinner's Snips
Cutter,
Power Cutter
All-Purpose Scissors