Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Board Anchor G4

Board Anchor G4
Sales Price: 8.99 SGD
Review Rating: 3.10
10 Customer Reviews
5 star 3
4 star 1
3 star 2
2 star 2
1 star 2
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
White board Wall hanging
3
From Japan
On 2017-07-10 14:38:23
It was easy to use. There was no particular improvement point.
This review is about item#10103055.
Board anchor drive
5
From Japan
On 2017-05-02 15:04:35
I used a variety of things but it is easy to handle because it keeps me on the board.
This review is about item#10103055.
Mounting of vanities
4
From Japan
On 2015-02-26 16:48:22
Because the wall was a board to install a new vanity table, it was dangerous if the vanity stand collapsed, so I fixed it with this board anchor. It is convenient because you can choose the size of the screw.
This review is about item#10103055.
Used for gypsum board
5
From Japan
On 2014-09-24 19:42:49
Strength preeminent. Easy to use.
This review is about item#10103064.
Installation of shelves to gypsum board
2
From Japan
On 2014-07-22 14:11:12
Because it is considerably poor construction, when driving into a plaster board (10 mm) with an electric screwdriver, one will be damaged for every three pieces. Moreover, after breakage, the damaged part got stuck in the gypsum board, so it was hard to remove.
This review is about item#10103064.
Installation of instruments on gypsum board
2
From Japan
On 2013-12-13 22:20:53
As it is screwed into the board, the tip of the board anchor may be caught and the board may be broken. When using it, open the hole of the size of the bit of # 2 Phillips screwdriver and screw it in. Also, although 4 mm screws are used for fixture mounting screws, it seems that the tip is not open to 4 divisions like the picture on the cover, so if light fixtures are used, when fixing a little heavy one, It is screwed in with a nipper at the tip with a slight break and it is screwed in (It may be opened with a 5 mm screw). When you put a break in the tip, you will hear a "snap" and tip open when you fix the instrument with screws. If you use with careful attention to the above, the price is also cheaper than the board fastener, it can be constructed more easily, the tip is opened to 4 divisions, so there are strengths, I think that it is a very good product. I think that it is sufficiently possible to attach instruments to the ceiling surface conditionally as long as the quality improves further in the future.
This review is about item#10103055.
Site work
5
From Japan
On 2013-10-31 07:15:19
I think the price is affordable and very good to buy. I will buy it again.
This review is about item#10103064.
For the foundation of the gypsum board pot for attaching the stairs railing
3
From Japan
On 2013-10-10 20:18:31
There is no problem in normal. Normal is the best.
This review is about item#10103064.
Installation of shelf support etc. on gypsum board
1
From Japan
On 2012-05-05 14:59:13
When screwing into the gypsum board, screws may break because of insufficient strength. As long as I tried about 25 pieces, one in two failed. If the anchor breaks in the middle of the wall hole, the broken anchor may fall apart and can not be removed from the wall successfully, and it will not be able to hit the eyes. Although it is written that there is no pilot hole, it was a similar result even if you try opening the underhole of the small eyes. It seems that the strength at the time of screwing is sacrificed because there are cuts in the four divided parts.
Attach to gypsum board, such as air-conditioner indoor unit
1
From Japan
On 2011-07-11 11:45:42
I tried installing it on a plain gypsum board with a charging screwdriver, but it got threaded when I entered about half of it, and it is the same kind manually. Poor poor product which is not useless at all. Compared to other companies it is soft and unreliable. Is there a problem with the material? .
1
Customer Who Viewed This Item Also Viewed
Anchor
Anchor Screw
Anchor Screw
Board Anchor
Drywall Anchor
Toggler
Wall Lock DX
Mini Auger Screw
Wall Lock DX
Toggler
Easy Time Board Anchor
Board Anchor, Noble Anchor
Mini Anchor Screw
Easy anchor