Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pin Punch

Pin Punch
Sales Price: -
Review Rating: 4.17
6 Customer Reviews
5 star 4
4 star 1
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Disassembly of gaming machines
1
From Japan
On 2017-07-30 15:48:03
It might be tough if it is this thickness, but I am glad if there is a product that does not bend more.
This review is about item#58392354.
Machine maintenance, overhaul
5
From Japan
On 2017-06-24 20:57:52
If you use a 5 mm pin punch when pulling out a 5 mm roll pin, it will be difficult to remove the pin punch when it is pulled out, so it will be a little narrower work
This review is about item#10231645.
Original punch, plus
5
From Japan
On 2016-06-07 15:37:46
It is convenient to use as other original punch, such as pulling a thin pin. Besides that, as a plus alpha, it is fine even if it is thin, so it can be used for everything as a little stick.
This review is about item#10231611.
Ikebana
5
From Japan
On 2015-04-01 16:29:02
Can not you make the thin part ahead longer?
This review is about item#10231602.
Extraction of spring pin
4
From Japan
On 2012-11-04 06:55:38
It bends when it hits diagonally. However, this thickness also turns or breaks for other goods which I have used until now. It might be tough if it is this thickness, but I am glad if there is a product that does not bend more.
This review is about item#10231602.
Disassembly of toys
5
From Japan
On 2009-04-07 14:18:46
Things are also very good, I think that it is excellent in cost performance.
This review is about item#10231593.
1
Customer Who Viewed This Item Also Viewed
Pin Punch Set
Pin Punch
Pin Punch
Pin Punch
S Bar
Pin Punch
Pin Punch
1.5mm Drive Pin Punch
Pin Punch
Knockout pin
Parallel Pinponchi round body
Parallel Pin Punch
Pin Punch
Pin Punch Set