Buy more than* S$200* and get FREE SHIPPING
Due to the national holidays as Golden Week, we will close 2018/4/28~2018/4/30 and 2018/5/3~2018/5/6.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of No.28 Hexagonal Shaft Tap

No.28 Hexagonal Shaft Tap
Sales Price: 10.99 SGD
Review Rating: 3.80
5 Customer Reviews
5 star 3
4 star 0
3 star 0
2 star 2
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Tap with drilling machine and lathe
5
From Japan
On 2017-02-11 15:04:39
I bought taps of all sizes, but it finishes cleanly. I can control the speed, but I can not reverse the rotation, so I attach a handle for the reverse rotation to the pulley of the drill machine. Those who are dissatisfied with the tap specification, this product is a hand tap just changing the shape of the general tap shank. By changing the shape of the shank, it was easy to install on the electric tool, but it is a manual type with a basic driver handle, a wrench handle, a T type handle for a hexagonal shaft, and so on. (It seems that T type handle used by MonotaRO is not handled with MonotaRO.) Also, because "the sharpness is about 4 to 5 mm from the tip" is a tap in the place called by tap , There are 5 pitches of staggering. (Since the tip is pointed except for + M8, it is not suddenly becoming thick.) If you wanted to shorten the sticky part, if you use the company "No.28 - S 6 hexagonal spiral tap" It is a short feel for one pitch. If you say that you break often, you can not do it with this product in a free hand with an impact driver, tap into stainless steel and hardened steel. To make a tap cleanly, you should use a drill stand (order code: 75806954or10921006) for the impact driver. Also, stainless steel is out of use. Also, at the time of pilot drilling, if you drilled a hole without cooling, you may get baked only on the side of the hole. Even if the material is soft iron it may become hard iron only in the pilot hole part. Then the tap may be defeated. For stainless steel, let's use the company's "titanium coating · point tap". When creating a new tap, let's repeatedly rotate forward and reverse, and screw it. (Like a hand tap ...) If you do tap at a stretch, let's make the pilot hole about 0.1 to 0.3 mm larger. (Depending on the screw size, high speed machining is also prohibited), you will lose the cheap buying.
This review is about item#10252365.
It is when screws are attached to the sashi when the screw is broken.
5
From Japan
On 2015-10-06 05:27:46
I am using it many times, but it is very good.
This review is about item#10252374.
Tap change of screws
5
From Japan
On 2014-10-16 18:01:28
It is possible to install on impact and easy to use or lengthy is also a good feeling to subscribe
This review is about item#10252374.
Threading with power tool
2
From Japan
On 2014-06-12 09:49:05
For this tap, when using it with a power tool, the sharpness is about 4 to 5 mm from the tip. At this point suddenly becomes thick and the depth of cut becomes deep, and if it can not be cut here, the thread of the member collapses and the hole becomes stupid. Hexagonal axis tapping is based on the premise of turning at a stroke with an electric drill or the like, I wonder why it is a middle tap. If the tip is thin like a rough tap and it gets gradually thicker, I think that it is possible for the screw to be cut cleanly even if not turning back and turning it off like turning the screw by hand . It is a good thing to be a hexagonal shaft, but this tap is just a conventional tap with a hexagonal axis, it is not thought to screw up at once in a power tool.
Screw of iron · SUS
2
From Japan
On 2012-01-22 00:56:11
Even if you are careful, it breaks considerably. I am troubled only by things that are not cheap. It is easy to use if you add ordinary tap to the impact chuck. By the way, I often use 6, 5, 4 mm.
This review is about item#10252374.
1
Customer Who Viewed This Item Also Viewed
Hex Shank Taps
Point Threading Tap
Hex Shank Tapping Drill
Hexagon-head axis spiral fluted tap
G bit
Pliers, long nose type
No.28-S Hexagonal Shaft Spiral Tap
Hex Axis Drill Tap