Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of No.29 Hexagonal Shaft Die Holder

No.29 Hexagonal Shaft Die Holder
Sales Price: 18.99 SGD
Review Rating: 3.00
5 Customer Reviews
5 star 2
4 star 0
3 star 1
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Motorcycle maintenance
3
From Japan
On 2017-12-12 14:56:16
I purchased it by looking at the review beforehand. Certainly, as the other person is saying, the inner diameter that the dice hooked was Φ 25.3. My dice is Φ 25.4 so we can use it by cutting with a lathe. There is no problem using it on the lathe.
This review is about item#10252401.
For processing
5
From Japan
On 2015-11-18 18:48:23
I did it by hand until now, but this is quick. About 1 cm from the tip of the rod is threadable. The dice which have several kinds had a diameter of 25.4 mm so they can not be used and shocked.
This review is about item#10252401.
Create millimeter · inch screw with lathe
1
From Japan
On 2015-05-19 11:03:16
"Onishi Kogyo No.29 Hexagonal Shaft Die Holder" is for 25 mm dies, but the inner diameter of the die part is 25.3 mm stronger and smaller than 1 inch (25.4 mm) dies, it is larger than 25 mm dice The center does not come out. There is no use only to sharpen the inner diameter with a lathe to make it for 1 inch (25.4 mm). In drilling machine, milling machine and lathe, it is shifted when using unadjusted parts. The screw thread correction can be used well with a handwheel.
This review is about item#10252401.
Correction of screw thread · New thread cutting
1
From Japan
On 2015-05-18 15:13:21
Although there is no problem in correcting the screw threads, in the case of new thread cutting, the center shifts. The reason is that the inner diameter of the die fixing part of the die holder is 25.3 mm or more. However it is less than 1 inch (25.4 mm) and inches type dice can not be used. (Not for inch screws.) Since the center of the die does not come out with the fixation of the die, the accuracy becomes less than class B in new thread cutting (creation of the original screw). Absolutely unsuitable for things that do not have thread cutting function on lathes. Manufacturers will not tolerate the error of only hand work as an acceptable range. Naturally, even if it is processed for 1 inch (25.4 mm) it will not even advise it. It seems that there is no schedule to improve the inside diameter to 25.0 mm or so close to high precision.
This review is about item#10252401.
Correcting the screw defect
5
From Japan
On 2014-04-30 08:23:35
It took time to rework, but thanks to the die holder, the efficiency got better! It is!
This review is about item#10252401.
1
Customer Who Viewed This Item Also Viewed
Screw Fixing Adapter
Thread Repair Die
Round Dies 25 Dia
Die holder
Die holder
Set File 5pcs
dice
Die holder
See Snake Micro Reel L100C Drum Only
Die Holder 25mm