Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of T-type wrench

T-type wrench
Sales Price: 6.99 SGD
Review Rating: 5.00
5 Customer Reviews
5 star 5
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Used for tightening the exhaust pipe holder of a 4-cylinder motorcycle
5
From Japan
On 2018-02-13 16:53:37
Exhaust holder tightening nut, the gap between the exhaust pipe and the frame is small, the socket wrench can not be used, and the long T-shaped wrench of the handle interfere with the front tire and it was difficult to tighten. This product solves these problems, it has become possible to loosen / tighten efficiently.
This review is about item#60940747.
Motorcycle Maintenance
5
From Japan
On 2018-02-02 21:16:16
It is easy to apply force, such as attaching a crankcase cover, and work efficiency also increases.
This review is about item#60940731.
During motorcycle maintenance
5
From Japan
On 2017-01-03 19:31:32
I bought it to replace the turnip sprocket. If you do not have this, removing the front sprocket cover thinks that those who maintain the Mendixai Mendixai Cub will certainly be happier if you purchase this product. This is a product that says so.
This review is about item#60940731.
To retighten the motorcycle
5
From Japan
On 2016-01-12 14:43:07
Even if it does not come out from the wrench box every time, it is very convenient if you know the size of regulation. I also use well other than motorbikes.
This review is about item#60940774.
For turning sprocket turnip
5
From Japan
On 2014-12-04 00:51:18
Although I have not used it yet, in the countryside "T-shaped 8 mm" in the home center is not 100% first. Even if there is, it should be "terrible high". I bought it with reference to the HP of one turn around Kabu Japan. The driving side sprocket seems quite tougher, and turning with the glasses wrench is a dimly severe appearance. It was good to purchase because there is an irregular tool size of 8 mm. Satisfied with the meaning 5 stars
This review is about item#60940731.
1
Customer Who Viewed This Item Also Viewed
TB T Type Box Wrench
BB T Type Square Box Wrench
YB Y Type Box Wrench
T form wrench
Long Reach T Handle Wrench
T-shaped handle 3 minutes 300
T-type wrench
Fast Turn T Form Wrench
T-shaped wrench short handle
LB L Type Box Wrench
Y-type wrench
Cross Wrench
T-Handle
T-box wrench header with 9mm
T Handle Wrench