Buy more than* S$200* and get FREE SHIPPING
Due to the national holidays as Golden Week, we will close 2018/4/28~2018/4/30 and 2018/5/3~2018/5/6.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of 9.5sq Bolt Twister

9.5sq Bolt Twister
Sales Price: 11.99 SGD
Review Rating: 3.50
6 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Removal of folded stud bolt of motorcycle engine
4
From Japan
On 2017-09-12 19:37:54
· I can work without anxiety that my legs are so short that they can break. - Since the insertion is 9.5 sq, it takes time and effort to tighten up again while working like a tap handle. · Although it seems that there is a meaning of prevention of breakage, it is not sure because the left screw catch is shallow and does not turn screws.
This review is about item#10315523.
Bike bolt
1
From Japan
On 2014-10-13 18:24:15
I pierced the M5 bolt tightly and it broke in only one time! It is! Applicable bolt, pilot hole is specified as well and usage is not wrong! It is! Of course the broken part remained inside and spent extra time! It is! I bought it for M6, but I am afraid to use it! It is!
This review is about item#10315505.
Unbolted bolt
5
From Japan
On 2014-10-08 17:53:11
I was able to work smoothly.
This review is about item#10315593.
Disk plate bolt
5
From Japan
On 2013-07-06 21:34:21
If you buy other soft items, it is safe to keep this cheap things broken so you can not help it anyway, but this item is a product we can recommend by far
This review is about item#10315575.
When removing the bolt which licks the thread
5
From Japan
On 2013-06-17 13:23:55
It was known that Yamaha motorcycle disk rotor bolt licked but my bike was no exception, I tried it after burning the bolt but I licked it Out of the six bolts wrench wrench If only a book is drilled to make a pilot hole and tried with a bolt twister, it is easier to disengage but it is better not to use besides the bokkin twisters. In a cheap twister, the twister itself may break and it may disappear any way Koken's bolt twister is a product that is made very sturdy and you can remove even bolts that are stuck together, it is a recommended product (⌒ 0 ⌒) b
This review is about item#10315575.
Racing cart
1
From Japan
On 2012-08-15 10:08:34
In the first use the drill part was torn out with one shot (broken). I used a short extension and T handle with a hole. I think that it was impossible to use it ....
This review is about item#10315514.
1
Customer Who Viewed This Item Also Viewed
Screw, Extractor Set
Extractor (spiral type)
Chain Bolt
Mesh disk
9.5SQ Twist Socket
(95002) clip
(91356) O ring
350g Test Hammer
9.5 sq Nut Twister
12.7 sq volt twister
Bolttwister Socket Set
Screw Extractor