Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Mr. Toolbag

Mr. Toolbag
Sales Price: 62.99 SGD
Review Rating: 3.92
13 Customer Reviews
5 star 4
4 star 5
3 star 3
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 13 of 13 Reviews
Equipment work
3
From Japan
On 2017-11-10 22:32:29
It's a bit too big to use. I wish I had checked the size well.
This review is about item#9207992.
Moderate size.
4
From Japan
On 2017-07-03 11:51:29
Basic tools are entering. If the impact driver is about other tools Even if there is, we will enter together. Shoulder belt is also useful
This review is about item#9207992.
Ventilation fan construction
4
From Japan
On 2017-01-26 17:58:25
The impression of seeing using this bag was very expensive. But, I have many pockets and I can put in various things. I used it in a ventilation fan but it is easy to use.
This review is about item#9208001.
To crimp the VA wire
4
From Japan
On 2016-10-09 17:49:36
I have seen this product at some construction site some time ago. They used this tool bag without using a waist belt. Therefore, I thought that the tool used in the type of construction will change. That's why I wanted one. I have not done any construction yet yet, I have set up various tools, but it may be ahead. Also, use this tool bag, I will write a review.
This review is about item#9208001.
Electrical construction
5
From Japan
On 2016-02-09 21:20:27
It is comfortable without having to organize the tool in the plug-in type and to retrieve the tool for ease of removal when using it
This review is about item#09208001.
Gas construction, electrical work, waterwork construction
3
From Japan
On 2016-02-04 19:46:14
The circumference of the bottom is breaking. A little more room for the size of the pocket.
Site work
2
From Japan
On 2015-10-20 08:44:58
I want a margin enough to accommodate the spray can in the outer pocket. If there are other colors Best
This review is about item#09207992.
Mechanical equipment maintenance industry
4
From Japan
On 2015-01-29 10:01:38
As my use, it is a pretty usable favorite product, but there are parts that I want to improve some points, I purchased twice, but I will not wait for a continuous purchase. Although there was a review that other people also bottomed out, there is a board in the bottom, but because the outer cloth rubs and tears, it becomes useless. In addition, when putting the bag outdoors in the rain, I think that the whole bottom gets wet and it gets wet to durability. Although it seems to be caused by storing the tool considerably, since the hook of the shoulder belt is made of resin, it will be broken if it is used for a while. Also, depending on the storage capacity, the shape of the bag will deform. At first it is a beautiful elliptical shape when viewed from the top, but after a while the bottom has an elliptical shape because of the plate, the top deforms to an undesirable oval shape close to a circle. Even if all the stored items are taken out and the shape is corrected, when carrying the tool and carrying it for about 2 days, it will be in an undesirable shape. Because there is more depth than the rucksack type bag, things do not fall, but it is really my favorite.
This review is about item#09208001.
Materials for high altitude work, tools
5
From Japan
On 2014-12-11 18:44:06
I bend it by matching the metal in the top with my waist and using it. I like the reasonable size and the durable place of the material.
This review is about item#09207992.
For tools used on site
3
From Japan
On 2014-11-20 12:25:06
I replaced it twice. The bottom was weak, and it went out in the same way. If you reinforce something, rubber etc, usability is good, so I will buy it once it is improved.
This review is about item#09208001.
Sheet metal tool holder, drill etc.
4
From Japan
On 2014-08-20 18:02:42
If partition partitions for separating inside the bag are sold separately The outer pocket is easy to put in and take out if there is a bulge in three dimensions. When thinking down to the shoulder like a shoulder which thinks that only one side is good, I think that it will not get tired if it is a shape that fits the line of the body like Kethel's tool bag
This review is about item#09208001.
Bring to construction site
5
From Japan
On 2014-03-21 10:34:09
It is easier to use than I thought! Satisfied! I am satisfied.
This review is about item#09207992.
Supplement and transport of tools necessary for the landscape industry
5
From Japan
On 2013-06-07 14:20:25
The texture is good and the material seems to be durable. It is convenient because it enters a lot in large capacity.
This review is about item#09208001.
1
Customer Who Viewed This Item Also Viewed
Tool Bag
Mr. Toolbag
Tool Bag
Mr. Toolbag
3D Tool Bag
Boston Tool Bag
Tool Bag
WAIST GEAR, Tool Bag
Tool Bucket
Tool Carryback
Pocket bag (round)
Work back
Mr. Toolbag
Tool Bag
Shoulder bucket
Oil filter
Tool Carry