Buy more than* S$200* and get FREE SHIPPING
Due to the national holidays as Golden Week, we will close 2018/4/28~2018/4/30 and 2018/5/3~2018/5/6.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Both Screw Bolts And Nuts

Both Screw Bolts And Nuts
Sales Price: 1.99 SGD
Review Rating: 4.17
6 Customer Reviews
5 star 4
4 star 1
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Metal working
5
From Japan
On 2018-03-04 22:50:30
It can be applied to various processing, anyway it is inexpensive and good. Please enrich the lineup of more sizes.
This review is about item#10979254.
For slide hammer production
5
From Japan
On 2017-10-17 10:48:47
Bolts for construction should be cheap. I bought it to make a sliding hammer which is a maintenance tool. Well, since the monotaro brand slide hammer is sold cheaply, it may not be necessary to make your own.
This review is about item#10979105.
Holding bolt for general purpose hydraulic cylinder
5
From Japan
On 2014-02-02 18:08:52
There are two threads crushed with ordering M16 x 600 8 pieces but there is no problem if you use it corrected.
This review is about item#10979254.
Working vehicle axle
5
From Japan
On 2014-01-12 17:25:46
It fits perfectly with the axle of the work vehicle.
This review is about item#10979281.
Used to join hole-down EX-M and girder
4
From Japan
On 2013-04-14 08:02:14
Although there was no problem with most items, there was a case that the nut did not turn by hand at the position of about 30 mm from the tip of the threaded portion, but abnormality was not examined on the screw in the appearance. As it is imagined, is not the plating layer concentrating on the protrusion (burr at rolling)? Is it?
This review is about item#10979245.
DIY
1
From Japan
On 2011-05-17 20:26:31
The thread was crushed in the middle. Returns are also troublesome and I managed to use it because I corrected for myself, but it is obviously a defective item. It is not easy to obtain this standard easily and it is inexpensive to overwhelm others, but is it that I am bad with it? Or should we recognize what Osaka people make like this? This time we attach it to ourselves, but it also concerns the reliability of your company selling, so we want to ask strict precautions for manufacturers.
This review is about item#10979281.
1
Customer Who Viewed This Item Also Viewed
Stud Bolt
Hexal Bolt Nut
Stud Bolt
Stud Bolt
Pulling Wing Plate Hardware
Steel Turnbuckle
High-strength flex both bolt
Square Washer
Round seat bolts
Fist Anchor Bolt
Roundlock Washer
Stud Bolt