Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of 600 V Triplex-Crosslinked Polyethylene Insulation Pvc Sheath Cable 600 V CVT

600 V Triplex-Crosslinked Polyethylene Insulation Pvc Sheath Cable 600 V CVT
5 star 1
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 1 of 1 Reviews
Wiring renewable energy! .
5
From Japan
On 2014-04-14 01:40:32
Although it was used for photovoltaic power generation, there are disadvantages that it is fairly hard and inconvenient to use, but the durability against high amperage is strong, the weather improves suddenly, even if high ampere power is generated, the place that does not do it is advantageous did. In terms of security and safety, I think that it would be better to have the margin of choice, and if it is to be added in the future, if it is within the allowable range of wiring, it can be raised to some extent. If the power operation is not performed within the allowable range of the actual wiring, the wiring is burned and there is no meaning to be installed, so it was the result which reached the present. But I think that safe and secure was obtained by choosing 600vCVT this time.
This review is about item#11136246.
1
Customer Who Viewed This Item Also Viewed
Pvc Insulated And Sheathed Cable, Cvv
Triplex Polyethylene Cable
News rat cable for low-voltage wiring
It'S Pvc Insulated Wire, Single WireIv 600V
Earth Leakage Breaker
Vinyl-insulated vinyl sheath cable (CVV)
Vinyl-Insulated Cable Pull-In DV-R