Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Mini Ball Valves , Hose Nipple Integrated

Mini Ball Valves , Hose Nipple Integrated
Sales Price: 9.99 SGD
Review Rating: 3.62
8 Customer Reviews
5 star 5
4 star 0
3 star 0
2 star 1
1 star 2
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Drainage work in aquarium
5
From Japan
On 2016-09-30 17:12:41
Branch off the middle of the outer filter hose of the aquarium, install this ball valve and drain it. It is very convenient to drain the aquarium easily by operating the valve. Since it does not install hose nipple, it seems that it is effective also for leakage prevention measures.
This review is about item#32621714.
During machine maintenance
5
From Japan
On 2016-09-25 02:54:55
Since the pressure resistance is 0.67, it is a little uncomfortable, so it may not be suitable for a compressor etc. that raises to 1 pressure. This time, since it was used for piping of carbon dioxide of 0.2, there is no problem.
This review is about item#32621705.
Floor warming work
5
From Japan
On 2016-02-05 21:20:27
Construction of floor heating As a supplementary heating machine of kerosene boiler, I made my own rocket stove As a waste oil drip valve to continue the combustion of this rocket stove I used it for oil volume adjustment. (Although rocket stoves are usually fueled with firewood, they will disappear if they do not have time to manage it, so firewood is burning while waking as a countermeasure, and oil is burned when going to bed. Continue to drip with potato stove Waste oil from waste oil cans Automatic extinguishing will be done when 15 liters disappear, even if fire is extinguished around 3 o'clock in the evening, warmth will last until 9 o'clock in the morning.
This review is about item#32621696.
Used as cock of oil discharge port
5
From Japan
On 2015-11-30 19:23:32
It is good without leakage.
This review is about item#32621696.
Low pressure gas
2
From Japan
On 2015-01-16 12:28:39
I bought a PT 3/8 male screw type, but it seems to be PS instead of PT. Moreover, because the screw part is short, putting it in the female screw of PT 3/8 is Yuruyuru. If we do not involve the seal tape so much, it will not be tightened.
This review is about item#32621714.
For air compressor
5
From Japan
On 2013-03-03 17:07:32
It is inexpensive and satisfactory.
This review is about item#32621723.
For manual opening and closing of oil supply used for drilling machine
1
From Japan
On 2012-03-30 14:50:26
The red plastic knob immediately broke. I am repairing and reinforcing it. It may be due to frequent opening and closing, please strengthen.
This review is about item#08206177.
Hose piping
1
From Japan
On 2010-12-24 16:26:20
I am worried whether the air volume can be secured because the inside diameter is narrow and the orifice is small. I think that it does not matter if limiting for use.
This review is about item#32621723.
1