Customer Reviews of Cns Bevel Black, With Blister Pack
|
Sales Price: 28.99 SGD
Review Rating:
![]() 5 Customer Reviews
|
|
---|
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Machine maintenance

From Japan
On 2017-02-27 14:37:06
It is easy to use, it is used for metal buffing and pre-sharpening of painting, cost decreases because reduction is fast.
This review is about item#32647562.
Iron handrail Keren work

From Japan
On 2015-06-23 17:15:54
I can not compare because I never used the wire type, but I got rust and old paint well as well. There is no problem regarding durability. Again, I think that the reliability of 3M items is high on all products.
This review is about item#32647562.
Peel off the skin.

From Japan
On 2014-10-22 19:28:30
Although I had a hard time peeling off the black skin, it was easy to peel off and it was useful.
Keren work of paint

From Japan
On 2014-01-17 14:10:51
Indeed the paint is easy to peel off, but wear is also fast so I do not want to use it next time in terms of cost.
This review is about item#32647562.
Rust on the substrate before painting, paint dropping

From Japan
On 2012-06-20 21:53:31
Used to re-paint the shovel loader's arm, one touch frame, lowering etc. Because it is lighter and more compact than the wire cup, it also goes into a narrow place. It is safe because there is no scattering. Since there is little catching on the edge etc. of the object to be polished, it is hardly fatigued since it is not shaken like a cup. There are few clogs and enough rust removal ability. It is also possible to leave paint in places that you do not want to peel off by how you put power. Also, if you are a bit cheaper you are not complaining ...
This review is about item#32647562.
1
Customers Who Viewed This Item Also Bought
<<
>>
(+) Bind small screw (stainless steel / head part white (only head part painted)) (pack article)
Osaka Spirit
4.99 - 5.99 SGD