Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Perfect Cushion Grip 2WAY Driver

Perfect Cushion Grip 2WAY Driver
Sales Price: 7.99 SGD
Review Rating: 4.00
3 Customer Reviews
5 star 1
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
When maintenance of equipment
5
From Japan
On 2015-12-15 10:02:29
Because the bit is ±, it is convenient for maintenance of American made equipment. It is also good work efficiency that bit can be used for impact.
This review is about item#32795576.
Temporary use for product development and battery replacement work
4
From Japan
On 2015-07-08 12:17:34
I use it when I want to see the inside by opening parts and machines while designing on the office desk. I put it in a pen insertion and keep it. I purchased it for the purpose only for purpose, I fascinated the place where Plus 1 to 3 can be used in common. Number 1 is perfect. Because point 2 is pointed, it hits the bottom of the groove of the screw, but it can be used without problems. Of course it should not be used in continuous work. No. 3 can also be used without trouble in the part where the screw is large and the torque is small. Just because the purpose is small torque applications for temporary use. If the grip is a bit thinner and lighter, it gets stabilized even if it is inserted in a pen, the pen insert is about to fall, it is a bit disappointing. If you take full advantage of the thickness of this grip and then tighten the second small screw in full swing, it is likely to break the groove of the screw head surely. Therefore is not it better to narrow the grip? I do not want the grip to divert the type, I want you to design it for exclusive use. The bit is so excellent that I really want you to sell only this bit. I would like to use it in combination with the new turtle's 5700 hybrid driver. In that case, since the minus size is the same size as the minus bit of 5700, I want you to make it small size.
This review is about item#32795576.
General car maintenance
3
From Japan
On 2013-01-24 19:50:22
In fact, I took it in my hand and felt "lighter than I thought." I think grip is also good. I have never put a lot of strength on it yet, I do not know the durability, but ease of use seems to be good.
This review is about item#32795576.
1
Customer Who Viewed This Item Also Viewed
Multi Purpose Screwdriver
Hybrid Grip Driver No.5700
Rubber Grip Screwdriver
Telescopic Driver, SUNFLAG
Hybrid Screwdriver No.5300
Perfect grip
8way Universal Driver
Bit Replaceable Screwdriver
Scaled Screwdriver
Replacement cushion driver
Commercial Grip Screwdriver