Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Mini Grinder, 100W

Mini Grinder, 100W
Sales Price: 219.99 SGD
Review Rating: 4.33
3 Customer Reviews
5 star 1
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Cutting of resin, outline processing
4
From Japan
On 2016-08-26 16:43:40
We are using a special machining table that can fix the router to the outer shape processing etc. of the resin flat plate. It is purchase of the third one for easy use. I broke two units, but I think that it processed too much without sufficient cooling for a long time.
This review is about item#32910866.
Drilling, cutting, cutting, polishing, rusting off, etc., etc. in various scenes of electric / electronic work.
5
From Japan
On 2015-06-27 17:04:10
Proxon (PROXXON) No.28400 is a high performance router among proxons. The mini router (hand router) owned by me uses Proxon except for toys. Maintenance of the mini router is better if you exchange each spindle and each bearing in 1 to 2 years depending on the frequency of use. There is also a way of saying that you do not maintain anything until the body is broken, but there is no good thing that the blurring becomes bigger by milling or turning machining, and the flat processing becomes dirty. When coming back from maintenance, it will be very quiet even at the highest speed rotation (about 20,000 rotations). Wind sound of the motor · It is only the sound of the router cooling fan that is connected to the motor. (Sound when new goods were purchased) While using my main mini router (No.28400) for repair (overfall), I use Proxon No. 28525 (MM100) purchased as a spare. Mini Router No.28525 MM100 is a spare to the end, so most people are asleep even if they drew a year. With Mini Router No. 28400 and Mini Router No. 28525, it is feeling that the No. 28400 is about twice as powerful as it is after all. I think that the mini router will be a life when regular maintenance is done. If you drill a hole in metal, No. 28400 is safe.
This review is about item#32910866.
Drilling of resin
4
From Japan
On 2013-10-27 17:44:45
It is the second one to purchase this tool. The fact that workers are used to it has become a major factor. It was just 10% off campaign and I tried to buy it. I am slightly dissatisfied that this type of rutual type is small.
This review is about item#32910866.
1
Customer Who Viewed This Item Also Viewed
Mini Router Kit
Rotary Tool 4000
Mini router MM20
Mini router MM30
Mini router LS 50
Multi Router Set
Mini Grinder, Body Only
High-speed rotary tool
High Speed Multi Router
Handy Multi Grinder
Mini Grinder Set, MM100
Carbide Cutter, 3 Type Set