Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of With Wide Monkey Wrench Color Grip

With Wide Monkey Wrench Color Grip
Sales Price: 22.99 SGD
Review Rating: 3.25
4 Customer Reviews
5 star 2
4 star 0
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Automobile
5
From Japan
On 2015-08-17 15:58:50
We are satisfied with the price Also lightweight, wide mouth, easy to use, but it is quite easy to use It is not used for places where large force is applied, but for normal use, there is no problem at all, it is grip, or a little more sure I will be saved if you do it
This review is about item#33033174.
Machine maintenance etc.
1
From Japan
On 2014-10-20 18:07:52
I think that there is no fault with Monotaro san ..... First I was surprised at the low processing precision! There is backlash of 1 mm or more as if the lower jaws were used up for many years (naturally, in the state just after arrival) I do not know whether it is a press mold or a mold but on the top surface of the most prominent it is about 1 cm in length of Ekbo There is a dent like the lower jaw, a sliding surface to slide? Cutting eyes of rough machine processing remained like a nail fillet. Even now, there are more decent things even for bargainless monkeys of no brands. It is a manufacturer product whose price does not change compared with other manufacturers, and this finish is honest, I can not help being disappointed and disappointed.
This review is about item#33033147.
Track maintenance and others
5
From Japan
On 2014-03-28 10:54:30
It was just right for size. Even without doing gloom, grip is listening and GOOD! was.
This review is about item#33033077.
Machine repair and maintenance
2
From Japan
On 2012-10-10 13:38:28
The opening adjustment is too loose, and the mouth opens as soon as it gets out of hand. When closing a bolt etc., when you put it on your head many times, you have to hold down the adjustment screw with your fingers. When trying to turn a tightened bolt, the angle on the side of the monkey side of the surface which contacted at the "point" was distorted slightly, as it was distorted to the shape of a horn of about 5 mm bolt. Maybe there was something wrong with how to use .... I think that fashionability is outstanding, but I think that it is not suitable for use with less load.
This review is about item#33033122.
1
Customer Who Viewed This Item Also Viewed
Wide Monkey Wrench
Monkey Wrench, Eco Wide
LIGHTOOL Monkey Wrench
Ultra Wide Monkey Wrench, Grip
Wide Monkey Short Type
Wide Monkey Wrench
Ultra Wide monkey wrench
Combination wrench
Light Monkey