Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Screw Fixing Adapter

Screw Fixing Adapter
Sales Price: 19.54 SGD
Review Rating: 3.67
6 Customer Reviews
5 star 2
4 star 1
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Bolt thread fixation
5
From Japan
On 2017-06-23 08:19:39
It is very handy because it can be rotated by hand as it is about screw thread correction of bolt. Even if I put it in the tool box with the commonly used dice in the adapter even if it does not bring out the die and the dice handle when I say that the nut is astringent even though it is not so frequently used It is a feeling that "I was looking for something like this" ♪
This review is about item#33127193.
Screw thread correction at all thread cutting
2
From Japan
On 2017-03-21 08:10:06
It's fine to have it compact, but on the contrary, the size is small, so the hand hurts when turning. It is fine to have a 17 mm bolt head, but I would like you to make it bigger and make it easier to grasp by hand with ease.
This review is about item#33127193.
Hub bolt screw thread correction
3
From Japan
On 2016-06-27 20:23:31
Especially it is easy to use without trouble
This review is about item#33127211.
As a die holder
4
From Japan
On 2015-12-09 21:54:37
The use feeling was good, but the set bolt is easy to relax. Although it may be relaxed in the same way with a dice handle, it seemed easier than expected. I feel it is troublesome to tighten it when tightened too tight, but I felt that adjustment was troublesome, but I think that it is very easy to use as a usability if you use it carefully.
This review is about item#33127193.
For hanging metal fittings of ceiling piping
5
From Japan
On 2014-10-13 08:07:45
It can also be used by hand turning without using a socket. Great.
This review is about item#33127184.
Used for screw thread correction of removed bolt
3
From Japan
On 2012-03-16 09:27:53
Attaching the target socket to the electric impact driver, we amend the screw threads of a large number of bolts together. The two screws on the side are easier to loosen, but as you tighten it strongly, the eyes of the dice become tight, so I look at the situation and use it while retightening.
This review is about item#33127193.
1
Customer Who Viewed This Item Also Viewed
Screw Thread Repair Kit
Screw Thread  File
Thread Restoring File
Thread Mate
Thread Repair Die
Die holder
No.29 Hexagonal Shaft Die Holder
INES blade
Ness One A
Die holder