Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Syringe Rubber

Syringe Rubber
Sales Price: 0.99 SGD
Review Rating: 4.44
9 Customer Reviews
5 star 6
4 star 2
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Repair of gypsum fertilizer and pesticide for measuring weighing spoyd
5
From Japan
On 2018-01-08 12:18:51
The chemical spyid was used for many years, the upper bellows part was damaged and the air leaked out, so cut that part and exchange it for spoil rubber. There seems to be no worry of getting in size with moderate tightness. Thanks, you can also use it for a while. It was saved because it was not sold to nearby shops.
This review is about item#33472126.
Nicotine Liquid Mixture
5
From Japan
On 2017-12-20 20:21:11
Since it was necessary 0.4 mL to make 10 mL purchase It has become possible to make it finely
This review is about item#33472047.
Used on Komagome pipette
4
From Japan
On 2017-08-05 12:38:58
The top is a bit thick. However, I am using it as it is not a concern to that.
This review is about item#33472153.
Apply solvent
2
From Japan
On 2017-03-22 10:24:32
I'd like to sell it with a set of glass Komagome pipette. I do not know well which size fits.
This review is about item#33472074.
Experiment
5
From Japan
On 2016-07-03 13:55:07
I could use it just like ordinary goods for the price. It was very good.
This review is about item#33472126.
Replace the old dropper bottle rubber
4
From Japan
On 2016-01-13 16:10:21
Since the rubber part of the dropper bottle is why the material is easy to degrade why somehow I exchanged it. Both the thickness and the outer diameter of the socket are large, so the lid screw becomes shallow and can not be used. Is it a splendid thing if you drop both with Thunder and bond with Bond 1530? It revived. (Although it seems better to buy it)
This review is about item#33472126.
Weighing aroma oil
5
From Japan
On 2015-07-26 15:58:18
I can use it without problems.
This review is about item#33472047.
Mix liquid and liquid
5
From Japan
On 2015-04-16 14:54:39
The material is a little soft and it seems that the force of sucking the liquid is somewhat weak, but it also has durability and is strong against solvents so it can be used with confidence.
This review is about item#33472074.
At work
5
From Japan
On 2014-01-10 18:59:49
I used it until now because it deteriorated and it became tattered so I purchased it here, I can choose the size and buy from the trader because it is expensive so I bought the wrong size as I did not hesitate, so next time it will be ml number I think I will purchase less people
This review is about item#33472153.
1
Customer Who Viewed This Item Also Viewed
Komagome Pipette
Dropper
Pipette LDPE
Pipets, Komagome, without rubber bulb
Rubber Dropper
Pipette Dropper Red
Komagome Pipette Graduated
Silicon Dropper
Color dropper
Red Dropper
Dropper for pipette
F Komagome Pipette, With No Pp Head
Lab run dropper
Silicon Color Dropper
Pipette Dropper 20ml
Komagome Pipette
Silicone dropper