Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of HI Different diameter socket

HI Different diameter socket
Sales Price: 0.99 SGD
Review Rating: 5.00
8 Customer Reviews
5 star 8
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Plumber
5
From Japan
On 2017-06-07 19:04:04
It can be used with confidence in the usual. Such things use only the manufacturer's products that can expect the obvious quality
This review is about item#34661042.
Plumbing work
5
From Japan
On 2017-06-07 17:29:16
It was completely usable without any problem. I want to use it from now on.
This review is about item#34661173.
Water supply piping
5
From Japan
On 2017-06-07 01:03:44
Since the product itself is a product of a first-class maker, it can be used with confidence. It is saved because it can be obtained cheaply and quickly.
This review is about item#34661076.
Piping work
5
From Japan
On 2017-01-17 20:42:38
It is also cheap and easy to handle with good precision and good stuff making.
This review is about item#34661042.
Distribution
5
From Japan
On 2014-03-21 21:44:21
Manufacturers are very satisfied with the fact that they can purchase at this price Manufacturer products can also be used for specific hazardous substances restriction (RoHS), so they can be used with confidence. Particularly for impact resistant fittings (HI) 65 A or more It is not in the home center etc. We are reliant on placing orders freely.
This review is about item#34661191.
Agricultural irrigation.
5
From Japan
On 2012-03-13 22:19:06
This socket connects the 20 mm diameter commonly used for PVC pipe around agricultural house and the next widely used 16 mm diameter. HI's material is strong against shock and freezing, so the price is a little higher than the VP material, but I mainly use the HI person outdoor. Because it is a size that seems to have many opportunities to use most in the different socket, we purchase it extra as stock.
This review is about item#34661042.
Agricultural irrigation.
5
From Japan
On 2012-03-13 22:01:04
It is a sogore thing that can be changed with this single socket from 20 mm frequently used to 13 mm at a stretch, and it is a very convenient socket if you have one. It is more beautiful than it looks with a simple addition and a finish added.
This review is about item#34661033.
Agricultural irrigation.
5
From Japan
On 2012-03-13 21:53:47
This standard HI series (dark gray) is slightly higher in price than VP (light gray), but it is highly resistant to shocks and freezing, so it is useful for outdoor etc. in the midwinter. In the past it was connected by VP and water cracked due to freezing, it changed from the crack, and later changed to HI. It is still strong without problems.
This review is about item#34661024.
1
Customer Who Viewed This Item Also Viewed
Vinyl Chloride Pipe HIVP 1m
HI Different diameter socket
HI Elbow
HI Valve Socket with Insert
HI Flange
HI 45 ° ELBOW
HI Bulb Socket
HI SOCKET
HI Water Plug Socket
HI Bulb Socket
HI Tees
HI Reducing Elbow
TS BULB SOCKETS (WITH INSERT)
HI Reducing Sockets
HI Reducing Tee
HI WATER PLUG SOCKET (WITH INSERT)
TS Different diameter socket
HI ELBOW