Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of PS Paper R

PS Paper R
Sales Price: 53.99 SGD
Review Rating: 4.86
7 Customer Reviews
5 star 6
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
To correct guitar fingerboard
5
From Japan
On 2017-02-03 17:54:52
It seems to be useful in guitar repair It seems that I cut the finger board quickly but it gets better and the accuracy gets better. After all I ordered AA abrasive BEST # 120 # 240 I ordered 400 # 400 so I'm just doing it with my hobby so it's about half the length It is just right if there is something It looks good and there is a use deadline It seems to be a problem of adhesive, but other 2 points may not be used because it is 40M
This review is about item#32584142.
Finish polishing woodworking work
5
From Japan
On 2016-07-14 23:21:11
I think that condition is good, shaving and durability are also good.
This review is about item#32582952.
Molding of wood for musical instruments
5
From Japan
On 2016-02-13 00:44:44
Compared to other sandpapers, this product is difficult to clog and it is hard to break, so it is appreciated that it can be used for quite a long time. When the eyes become rough, the file file is easy to peel off when folded or folded, but this product is very useful because it is durable even if it is folded. Because it's a bit better, it will be more helpful if the price is cheap, but I am satisfied with the cost performance as well.
Polishing
4
From Japan
On 2016-02-09 19:46:09
It is good if there is goods of 5 m unit. If it is 25 meters it will be for the whole lifetime.
This review is about item#32582952.
Race Car Carbon Kevlar Product Finish
5
From Japan
On 2015-11-10 08:11:58
I used various roll paper up to now, but it is the highest quality, durable and long lasting paper. Three times of other companies' paper (including certain famous manufacturers) will last long. Performance is overwhelming. I wish I knew this sooner.
This review is about item#32584176.
Shine such as trees and FRP
5
From Japan
On 2015-03-10 13:14:03
Easy to use, there is strength after folding. Kovacs etc. will be separated into two.
This review is about item#32584142.
Finishing at the time of string instrument production etc.
5
From Japan
On 2012-05-09 03:31:57
It is used for ruling of fingerboard of stringed instruments and finishing of bonded part, but it is very convenient because it is difficult to clog and can be well removed for the proportion of the bandage. Earling of the fingerboard part of the musical instrument also has adhesive strength like a seal, so it can be stuck directly to the jig so work efficiency is up. However, if there are too many sticky things that the file is left in the jig when sticking it to the jig of aluminum or peeling it, it takes time to peel off. I will not say it if you can improve the peeling easily while leaving the current adhesive strength.
This review is about item#32584167.
1
Customer Who Viewed This Item Also Viewed
Magic type sandpaper HNAR type roll (100-mm width)
Magic type sandpaper HNAR  roll (75-mm width)
Sanding Paper,
PPS paper R
Sandpaper Rolls
PPS N
  • PPS N
  • FUJI STAR (Sankyo-Rikagaku)
  • 67.99 SGD
Dry Paper Disc, 75mm Width
Pop-up roll paper
Stikit Gold Finishing  Roll
Dry Paper Disc