Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Rotary Nut Coupler

Rotary Nut Coupler
Sales Price: 28.99 SGD
Review Rating: 5.00
2 Customer Reviews
5 star 2
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
Used for hose for air ratchet connection
5
From Japan
On 2015-03-18 16:30:41
Since the air ratchet is often used to thrust a hand in a narrow place and change his posture, the hose is liable to twist and it is troubled because it causes breakage and catching, but this coupler solved it. Also there is a spring part so the hose does not break at the base of the coupler, this also has an effect. I am thankful that there is a coupler for a thick hose with an outer diameter of 14 mm and an inner diameter of 10 mm used for impact.
This review is about item#34730595.
Home use DIY car · Home repair etc. General work (Equipment: spray gun, airbrush, sander, impact wrench, etc.)
5
From Japan
On 2014-07-23 08:29:52
We use two old and new air compressors and two auxiliary tanks for private use DIY. The old urethane hose enters the habit so badly but still the connection of the comp tank is acceptable. The final connection from the tank is a 10 m · 20 m soft air hose. However, even if it is a soft type, twisting becomes worse when using around spray gun etc. moving around. As a result of various studies, I decided to try this rotary nut coupler. Immediately after arrival, we started repairing the entrance door of the house and used it with double action thunder spray gun. It is a wonderful feature. Bearing effect and hose breaking prevention spring exercised great performance. It is not involved at all. Every time I move it exquisitely turns around by hand and quickly eliminates twisting. The work progressed very smoothly. Although there are some without springs in the series, we recommend this spring type together with hand filter. In addition, it seems to be using numbers, so if the price is less than 1000 yen it is the best.
This review is about item#34730586.
1
Customer Who Viewed This Item Also Viewed
Rolling Ball Plug
Lock Coupler 200
Duster Coupler
Urethane Hose Coupler
High coupler twist plug
Free Angle 2 (rotating plug)