Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Simring X1 Inner Diameter 12phimm Stainless Steel Material, SUS304

Simring X1 Inner Diameter 12phimm Stainless Steel Material, SUS304
Sales Price: 0.99 SGD
Review Rating: 4.50
4 Customer Reviews
5 star 3
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Adjustment of rattling of the brake bar
3
From Japan
On 2017-11-30 11:11:20
Since there was rattling at the time of exchanging with the outside brake bar, purchased as a backlash. Although additional fee was generated as it was a carry-on part, we were satisfied with the customer.
This review is about item#34799475.
Mini lathe feed screw thrust adjustment
5
From Japan
On 2015-11-03 21:04:20
It can be bought in small quantities (1 sheet) unit so it is saved. However, although I purchased t0.02 / t0.10 / t0.15 / t0.20 several pieces at a time, I was sorry that this was split into three parts. Since then only the part number is printed in the bag, I think that it is just a little more pleasing if the thickness is written.
This review is about item#34799046.
bike
5
From Japan
On 2015-06-17 19:37:33
In other stores on the other shops these things are hard to sell because they are not readily available, so it really helps me. Goods are also good quality.
This review is about item#34799475.
Adjustment of clearance of machine parts
5
From Japan
On 2013-09-06 13:48:30
It is good to be able to buy a small amount cheaply, but I want you to ship earlier.
This review is about item#34799186.
1