Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of LED Vehicle Height Lamp

LED Vehicle Height Lamp
Sales Price: 23.99 SGD
Review Rating: 4.00
4 Customer Reviews
5 star 2
4 star 1
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Truck's car high light
2
From Japan
On 2016-03-30 14:02:00
In the car high-light of LED, it is a type in which the unusual base and cover are separated, and it can be confirmed in the product image. The screws on both sides fix the lens and the base screw only. Screw holes to fix the base is a type that utilizes a hole of 80 mm width attached to the base only. I thought that the lens and the base were an integral thing for the LED, so I ordered it, so I was surprised to be honest. It is a type that can not be seen in the LED car highlights that I have used so far, so I have to fill in the comment section again because there is a possibility that someone who is confused after purchasing will come out. The item description is too simple too. We measured the dimensions only and ordered it easier Here is non-existence but I think whether there is a more detailed item explanation.
As a repair of a car high light of a large car
5
From Japan
On 2015-10-28 17:26:11
Although there is no dissatisfaction about this car height light, I want you to know finely because there are things that do not have installation size etc. on other goods.
This review is about item#34814376.
Truck's car height light
4
From Japan
On 2014-12-06 15:36:57
In order to enhance waterproofness, it is installed after applying silicone bond etc. at the time of installation, so I'd like to increase waterproofness. You can use genuine accessories from the beginning.
This review is about item#34814376.
Used as a marker for heavy duty trucks
5
From Japan
On 2014-11-18 18:22:30
I bought it for repair that the marker was broken only on one side. Although it was planned to buy two left and right, it was the same type as the marker currently arriving, so it was only one.
This review is about item#34814376.
1