Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Flattened Can, With Chemical Cock

Flattened Can, With Chemical Cock
Sales Price: 39.99 SGD
Review Rating: 2.33
3 Customer Reviews
5 star 0
4 star 1
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Emergency water container
4
From Japan
On 2016-11-11 19:15:57
Even when the cock is fully opened, the flow rate is low
This review is about item#34877911.
Temporary storage of parts cleaner
1
From Japan
On 2015-08-13 01:08:28
It's been three months since I used it, so it's a cock and a nozzle? The place broke and the inside spilled ... It depends on the contents, but it is a great loss ... The cook is a bad feeling from the original ... so the cook is a neck! Moreover, it can not be exchanged, so the tank is useless.
This review is about item#34877902.
For subdivision of isopropanol aqueous solution
2
From Japan
On 2012-02-02 12:46:23
It seems that the accuracy of the upper wide end cap or the main body or both is not so good, there is packing in the cap, and even if sufficient tightening is done, the contents will leak out if you lay the tank sideways. There are also a lot of Bali at the time of molding, and at this price it is about this level. There is no leak from the red cock. The polyethylene cap attached to the cock may be in close contact with the cock, but once removed it is quite tight. I thought whether it was necessary to have fingers hanging on the cap part.
This review is about item#34877911.
1
Customer Who Viewed This Item Also Viewed
Plastic Tank
Lever Screw Cork
Tapered Jar Square, PP, No Scale
Square Bottole 20L, Tap
With wide-mouth bottle chemical cock
Flat Plastic Tanks
MJ tenor Chemical cock (liquid remaining prevention)
Gas Can Tap