Customer Reviews of D-Ring Files, S Type
The reviews are automatic translation.
Showing 1 - 12 of 12 Reviews
Managing documents

From Japan
On 2017-07-29 08:10:19
The file itself is light. Also, it is easy to use the ring opening with one touch.
This review is about item#08251537.
Save studied print data by grade separately

From Japan
On 2017-05-20 06:36:01
In the shop, there are abundant colors that can not be obtained, it is easy to separate, easy to open and close with one hand, and the documents are difficult to fall out because they are firmly engaged.
This review is about item#08251546.
Used in customer account

From Japan
On 2017-04-24 12:45:13
I think that the ingenuity of the D ring has been stifled from the old Kokuyo file, which is good. Just opening it seems to be narrower than the old file.
This review is about item#34946073.
Document storage

From Japan
On 2017-03-08 13:20:20
The D ring has a structure that can be easily opened and closed. Since paper restraint is also attached, it seems that the documents can be kept cleanly.
This review is about item#34946143.
For document arrangement

From Japan
On 2016-05-03 16:19:40
I hold down the D ring with the front cover, so the paperwork is nice.
This review is about item#34946177.
Organizing documents

From Japan
On 2014-09-12 15:48:16
When closing the file, the ring fits into the hole, making the shape of the file difficult to collapse. I purchased it before, but it does not collapse at all even after one year. It would be appreciated if you could make it a little cheaper if possible.
This review is about item#08251537.
Document arrangement

From Japan
On 2014-02-04 09:22:50
Easy to use
This review is about item#34946012.
File General Ledger.

From Japan
On 2013-08-09 08:53:21
I want to file a general ledger for one year, but I'd like the ring size to be bigger, but it seems not to be this type. Is it impossible to enlarge the ring so that the thickness of the file does not become too thick?
This review is about item#08251537.
Classification of documents and materials

From Japan
On 2013-03-11 13:18:35
It is easy to open and close the ring. Useful for organizing documents of moderate quantity. Easy to take out from the shelf. I think that it is convenient and well devised for preservation and management of documents by using color classification together.
This review is about item#34946055.
Filing of accounting materials

From Japan
On 2012-12-20 12:16:29
It is good to make it hard to break and abuse as it is solidly made with plastic files.
This review is about item#34946003.
Filing of work instructions downloaded on the Internet

From Japan
On 2012-09-14 14:32:06
Together with orders of 100 brands of clear file of no brand, when using it, it protruded from the file. Were you using Kokuyo made without sticking out? I thought. Was the delivery status bad? It was disappointing that there were scratches. One was replaced because the ring was not engaged and it was a defective product. Exchange was smooth and correspondence was good.
This review is about item#08251537.
Filing on-site document

From Japan
On 2012-04-19 13:47:15
I have been using it for several years. It is outstanding.
This review is about item#08251537.
1
Customers Who Viewed This Item Also Bought
<<
>>
Hex Socket Button Head Screw, Button Cap Screw, JIS-B1174, Stainless Steel, Small Box
Osaka Spirit
50.99 - 159.99 SGD