Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Brass Needle Valve, 10K

Brass Needle Valve, 10K
Sales Price: 12.99 SGD
Review Rating: 4.00
5 Customer Reviews
5 star 3
4 star 0
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
I am using it when adjusting the trace of water
5
From Japan
On 2018-04-09 16:10:12
Although it is using it for a long time, it can be used without particular problem.
This review is about item#35057206.
Used as inlet side air regulator of air impact wrench
5
From Japan
On 2016-11-17 20:34:51
Used as an air regulator on the inlet side of the impact wrench. It can be adjusted steplessly at hand, and there is no problem with the air volume at all.
This review is about item#35057206.
For gasoline flow adjustment
2
From Japan
On 2016-09-08 16:47:29
Since it is not yet full-scale operation, it can not be said clearly, but it seems that opening and closing is realized that the flow rate can not be adjusted.
This review is about item#35057197.
Adjust oil flow rate
3
From Japan
On 2016-05-24 21:00:51
In particular, there is no dissatisfaction or inconvenience
This review is about item#35057197.
PVC welding, air brush volume adjustment.
5
From Japan
On 2015-07-25 09:14:30
As I saw the needle part with 1/4 of the commodity, I was a bit small, so I was worried about the air volume but there was no problem at all when installed and tested. We use the pressure gauge and this product under the shape called the coupler in the work room through piping from the wall to the wall through the wall. I put a regulator on the piping from the compressor outside the room and put it in the room. I think that the compressor was the correct answer using this product which makes it possible to turn on and off the driving in the room and adjust the delicate air volume in the room.
This review is about item#35057206.
1