Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Air-only polyurethane tube

Air-only polyurethane tube
Sales Price: 11.99 SGD
Review Rating: 4.60
5 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Used for pneumatic piping.
5
From Japan
On 2018-03-13 10:41:14
It is cheaper than the UB series. The UBT series has just started using it, but its durability is evaluated in the future. Worry about hardness · bending resistance · environmental resistance (especially sulfide · peroxide gas atmosphere etc.). Those manufactured overseas will crack due to hardening embrittlement and cause air leakage, but we are expecting how far we can withstand such an environment.
This review is about item#87890476.
It was used for new plumbing
5
From Japan
On 2017-09-01 17:12:01
I always use it! I can trust! Piping work is also very easy.
This review is about item#87890415.
Machine Tools
5
From Japan
On 2016-09-29 17:50:55
I have been using other manufacturers until now, but I think that this one is cheaper and quality is equivalent. I use it for machine tools at 10 meters at a time, 20 meters at a time, so I would like to use the cheapest one from this manufacturer. The color is also cool and it is satisfying.
This review is about item#87890467.
As equipment connection hose
4
From Japan
On 2016-08-18 16:19:45
Easy to use, moderate hardness There is softness.
This review is about item#87890521.
Air piping of radio controlled airplane
4
From Japan
On 2015-01-18 17:14:40
Especially without any problems, 1 volume 20 m is too long. It is best if there are 5 m or 10 m.
This review is about item#87890275.
1
Customer Who Viewed This Item Also Viewed
Polyurethane Tube Black
Fluorine Resin Tube, PFA
PU Tube
Cable Ties
Yodoflon PTFE Tube
Yodoflon PTFE Tube 16x14
Soft Nylon Tube