Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Light Coupling Socket Straight Screw Type

Light Coupling Socket Straight Screw Type
Sales Price: 9.99 SGD
Review Rating: 4.14
7 Customer Reviews
5 star 3
4 star 3
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Production of carbonated water
4
From Japan
On 2018-02-26 15:20:40
Although screws are short, it is okay to remove the packing and tighten it tightly
This review is about item#35315305.
Production of carbonated water
5
From Japan
On 2018-01-31 10:52:05
I bought it because I tried to make my own carbonated water. The screw length was short and it could not be installed unless packing was removed. The feeling of use is very well Repeat as it is without pressure leak as it is.
This review is about item#35315323.
Creation of carbonated water with carbonic acid gas
5
From Japan
On 2017-09-07 15:46:46
With solid build, no air leaks, you can use with confidence.
This review is about item#35315305.
Purchase for making carbonated water
5
From Japan
On 2017-09-05 14:56:49
I think that desorption with the light coupling plug elbow one-touch fitting type is also easy and very good. I think that the feeling of security will increase if the screw part has a length about twice as long.
This review is about item#35315323.
My creative work by a carbonated water maker
4
From Japan
On 2017-01-31 13:54:46
The screw is somewhat short. I can manage to put a nut on it somehow, but I guess it is safe to have 3 mm more.
This review is about item#35315323.
Indoor piping
2
From Japan
On 2015-07-23 17:11:44
M5 screws are cut and fixed with nuts, but it is difficult to pinch something between screws because it is short, I think that it is dangerous if it is high pressure. It seems to be a type that connects directly to equipment and piping.
This review is about item#35315305.
To make carbonic acid
4
From Japan
On 2014-09-29 21:06:39
In the installation, the screw part was short, the seal was removed and a little cap was scraped and attached. I am satisfied with feeling satisfied.
This review is about item#35315323.
1