Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Specially Selected Printed Plywood

Specially Selected Printed Plywood
Sales Price: 369.99 SGD
Review Rating: 4.00
5 Customer Reviews
5 star 2
4 star 1
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Office interior
3
From Japan
On 2015-08-17 10:45:51
Although there was anxiety such as texture only with the image of the net, the actual thing was as expected and it was good. However, although there was individual variation, it was not understood at first glance, but there was something different in color when there are something that was sorry.
This review is about item#35603154.
Residential wall renovation work
3
From Japan
On 2013-09-05 19:45:38
I do not know if it is in transit, but the corners of the four corners are rounded. I think it would be better to apply a more durable horn. There was no problem on the surface / back surface.
This review is about item#35603145.
We installed this veneer on the old silicon wall, and western style
4
From Japan
On 2013-02-04 16:29:49
The vertical type is common for grooves, but the horizontal type is suitable for use on the stairs. It is convenient to arrange both types and display it in the item description.
This review is about item#35603136.
Used for installation on the interior wall of the house.
5
From Japan
On 2012-10-14 23:48:13
I think that it is a very good product. Especially, I chose the type 60 number very much like n color pattern.
This review is about item#35603154.
To cover the soil wall.
5
From Japan
On 2011-11-05 16:38:34
I think that it is a product with very high cost performance.
This review is about item#35603136.
1