Buy more than* S$200* and get FREE SHIPPING
Due to the national holidays as Golden Week, we will close 2018/4/28~2018/4/30 and 2018/5/3~2018/5/6.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Glass Tube Fuse 25mm

Glass Tube Fuse 25mm
Sales Price: 6.99 SGD
Review Rating: 4.60
5 Customer Reviews
5 star 4
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Maintenance of old car two wheels
5
From Japan
On 2017-07-06 15:03:03
Quality is also good and it is saved for cost. It is unexpectedly very thankful that there are shops with 25 mm tube fuses.
This review is about item#35509004.
Maintenance of old car two wheels
5
From Japan
On 2017-06-14 14:38:40
Evaluation comment can not be done yet because it is before use, but 25mm glass tube fuse was quite absent at the shop front. It was saved.
This review is about item#35508995.
Old motorcycle maintenance
5
From Japan
On 2016-02-07 16:23:07
The short type of 250 mm is saved because it is not placed in ordinary mass merchandisers.
This review is about item#35509022.
Used for old two wheels
3
From Japan
On 2015-07-24 17:08:04
Because the old turnip is 25 mm · 7 A designation. When I looked at the picture, I was not familiar with medium-sized slender board wire fuse for home appliances, so it was uneasy, but since it is "auto fuse" purchased on trial. After all, it is 125 v 7 A with a line fuse, and the hand held tester does not know the difference from the 12 v product. I have tried it for the current car for two weeks but there is no problem at present. If possible, please explain whether this line fuse is different from the conventional 12v version · What is the exchange problem?
This review is about item#35508995.
Motorcycle repair
5
From Japan
On 2014-04-11 14:07:41
It is an ordinary tube fuse. Since this model size is getting out of line at the shop front, it is very much appreciated that it is always on sale at all times.
This review is about item#35509022.
1
Customer Who Viewed This Item Also Viewed
Pipe Fuse
Fuse
  • Fuse
  • SANWA ELECTRIC INSTRUMENT
  • 0.99 SGD
  • 4.769230(13)
Glass Tube Fuse
Glass Tube Fuse 0.5A 250V
Mini Glass Tube Fuse
Glass Tube Fuse 30mm
Mini Tube Fuse Set
Bike Fuse
Glass Tube Fuse
Terminal bolt & nut
Glass Tube Fuse