Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Galvanized Steel Flexible, Flexible Iron

Galvanized Steel Flexible, Flexible Iron
Sales Price: 36.35 SGD
Review Rating: 4.60
5 Customer Reviews
5 star 4
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Ventilating fan duct
5
From Japan
On 2016-06-23 18:10:03
You can freely take the ventilating fan duct with the ceiling behind.
This review is about item#35594955.
Kitchen range fans piping
5
From Japan
On 2016-04-11 16:02:05
I am using it frequently in our electric construction work. I think that it is good because there is nothing to crush soon like an aluminum duct although it is a little hard and not stretched. It is easy to cut hands at the cut end, Aluminum duct has little such a thing, but it is hard to handle such a surface a bit. Hopefully it will be easy to extend a little more.
This review is about item#35594955.
Kitchen ventilation duct
5
From Japan
On 2016-04-09 15:48:39
Though selling in general, the price is high, but it is worthwhile, it is strong and it is saved.
This review is about item#35594955.
Kerosene boiler chimney
5
From Japan
On 2014-10-06 14:01:06
There is no particular problem in terms of performance.
This review is about item#35594946.
Range hood duct construction of wooden building
3
From Japan
On 2014-08-30 11:10:08
The length was short, so it was nice to have few left over
This review is about item#35594955.
1
Customer Who Viewed This Item Also Viewed
Flexible Duct Hose 3m
Flexible Hose
Flexible Aluminum, W Type
TOYO Duct AL-N 4m
Compact Flexible Duct
Spiral Nipple
Spiral Nipple
Spiral Elbow 90 Degree
Aluminum Flexible Duct
Spiral Reducing Joint
Spiral Elbow 45 Degree
Iron flexible Fujifureki T
Rotary type flexible duct
Tiflex Hose V series PAL type
Tiflex Hose V series PAL type