Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Spiral Tee

Spiral Tee
Sales Price: 26.99 SGD
Review Rating: 4.00
5 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Piping work
5
From Japan
On 2016-11-03 19:42:46
Cost performance is good
This review is about item#35595113.
Duct branch
5
From Japan
On 2016-04-05 17:28:57
It can be used normally
This review is about item#35595104.
Exhaust extension in plant
1
From Japan
On 2015-12-10 11:49:49
Variations in the hole diameter were large, and when fitting the aluminum bellows duct, there was a thing that could fit smoothly and there was a thing (place) that did not enter, and it had to do things like snapping in the duct and holding it with tape. I think that it is easier to use if the diameter tolerance is made smaller.
This review is about item#35595104.
Kerosene boiler chimney
5
From Japan
On 2014-10-06 13:59:48
There is no particular problem in terms of performance.
This review is about item#35595095.
duct
4
From Japan
On 2013-07-08 09:11:40
I could buy it cheaply
This review is about item#35595095.
1
Customer Who Viewed This Item Also Viewed
Flexible Hose
Y Spiral Tube
Spiral Nipple
Spiral Nipple
Spiral-Y
Spiral Elbow 90 Degree
Spiral Reducing Joint
Spiral Reducing T
Spiral Reducing Y
Straight pipe cap
R tube (reducer)
Cap
Y tube
Fixing color
Air Volume Contorol Damper
Spiral Nipple
Press elbow 90 degree
T pipe