Buy more than* S$200* and get FREE SHIPPING
Due to the national holidays as Golden Week, we will close 2018/4/28~2018/4/30 and 2018/5/3~2018/5/6.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Resin Bearing DU, Outer Ring U-Groove Type) TYPE4

Resin Bearing DU, Outer Ring U-Groove Type) TYPE4
Sales Price: 1.99 SGD
Review Rating: 3.60
5 Customer Reviews
5 star 2
4 star 1
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
work
3
From Japan
On 2016-07-05 12:48:16
Although the price is cheap, it is usable normally.
This review is about item#35778102.
Machine oil is used for the transfer machine part which can not be used.
4
From Japan
On 2016-06-22 14:46:42
I want a size of 50 mm in diameter.
This review is about item#35778102.
Hand lift parts
1
From Japan
On 2016-04-08 09:00:27
The strength of the bearing part was weak and it broke in several days.
This review is about item#35778102.
I used it for an old sliding door of TOSTEM
5
From Japan
On 2016-03-02 16:22:33
We used it for the old sliding door car of TOSTEM. (It is a door before the Heisei first year) Although the tire size was 36 mm specification, the difference between the height adjustment function on the bracket side and the radius 0.5 mm did not become a problem at all. Even though I heard from Rikkilu (formerly TOSTEM), there are metal fittings but there are not only tires. Since ASSY is about 2,500 yen, it was good that only cars could be exchanged. Because it was a heavy disaster-prevention glass door, the initial tire was sliding while playing hard, but this time the tire does not sound so much. I would like to purchase again as the bearing decreases.
bearing
5
From Japan
On 2014-03-20 12:41:39
no problem
This review is about item#35778093.
1