Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Mowing Nylon Cutter Round

Mowing Nylon Cutter Round
Sales Price: 2.99 SGD
Review Rating: 3.67
9 Customer Reviews
5 star 4
4 star 1
3 star 1
2 star 3
1 star 0
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Of course it is grass cutting.
5
From Japan
On 2018-04-24 15:03:38
3 mm round shape is hard to find in home centers and JA. It is cheap and strong. I will also order the next.
This review is about item#60958161.
Weeding work
5
From Japan
On 2017-06-14 21:09:59
easy to handle. Improvement points ............ I do not think so!
This review is about item#36728754.
Mowing
5
From Japan
On 2017-05-17 15:07:47
Especially with normal chip saws such as masonry and block stacking, we use it in difficult place. Mowing can be done smoothly without hurting the machine. Even if it is thinner than this, it is not good even if it is thick, and it is just good thickness.
This review is about item#36728754.
We mainly use it to weed the boundary with concrete.
4
From Japan
On 2016-07-17 20:22:49
I was using 2.7 mm, I should try using 3 mm to try ~ Engine horsepower may be insufficient? I thought that I used it and it was able to be used without difficulty if raised a little. After cutting it became a place to shave a little to the ground beautiful Sappori code is cheap but I think that this was a good shopping. Is it too fast from purchase to product delivery? It was one day earlier than expected. Thank you very much.
This review is about item#60958161.
Grass cutting at the parking lot
2
From Japan
On 2015-10-20 23:30:20
Have you broken so much? I could be as good as I thought. Especially for a moment if you hit the grass that seems to be slightly hard. In this case, even if it is cheap, hourly salary will be higher. I will not buy it anymore.
This review is about item#36728745.
Mowing at home
3
From Japan
On 2015-04-16 11:58:46
Because it is the most ordinary and cheap, everyone will buy this at the beginning, but ... you still like rectangular titanium (?). It is the best reason why slippery slipping and hard to wind up.
This review is about item#36728754.
Mowing
2
From Japan
On 2013-11-12 10:21:53
I bought it because it is cheap, but it is clearly pricey. Instead of wearing and tearing immediately, the grass is not nice. It might be a good idea to cut soft grass so that it strokes.
This review is about item#36728754.
Use for reaping weeds such as roads and fields
2
From Japan
On 2013-10-07 19:58:17
It is worn out as soon as the cord that you can use with confidence to cut grass such as Ishigaki frequently used from spring to early winter hits stone etc. If you do it twice as long as now it will improve workability Price will be the same length I would like about 500 yen
This review is about item#36728754.
Weed removal in road guardrails
5
From Japan
On 2013-07-17 08:26:25
It can be used without fear of weeding out under metals · concrete environment at low price at 70 m.
This review is about item#36728754.
1
Customer Who Viewed This Item Also Viewed
Mowing Nylon Cord X Type
Nylon Cutter Basic
Nylon Cord Twist
Nylon Cord HI-X Type
Nylon Cord HI
Nylon Cutter Hex
Power Nylon Cutter
String Trimmer
Nylon cord star 2.7mm
Mowing Nylon Cord (Round)