Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Center Slide Rail

Center Slide Rail
Sales Price: 4.99 SGD
Review Rating: 4.17
6 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Withdrawing my own work
5
From Japan
On 2017-02-02 17:50:51
Since I can put about 15 kg of things, I tried using two centimeters instead of the center. It seems the movement is a bit heavy, but it may be a problem of parallelism between the rails. It is likely to be used without any problems with respect to other play, strength, etc. To fix it, truss screw was used for fixation.
This review is about item#36291123.
Create slide shelf
5
From Japan
On 2015-11-13 20:43:26
Because the bottom draw rail is not sold easily even at the home center it was good that I could purchase 2 slide shelves of finished satisfactory finish with decorative board using 2 pieces
This review is about item#36291157.
Slide shelf
2
From Japan
On 2015-11-07 19:10:13
Even if you do your best, the inner rail and the outer rail can not come off. Since it can not be helped, we installed it for the time being, but it is unstable because the edges can not be fixed. I used the recommended bevel head tapping screw but it hits the rail. I thought that the slide shelf I was thinking was completed, so it was good, but I will look at the situation for a while.
This review is about item#36291157.
I would like to try using my own for the XY table on the drill table.
5
From Japan
On 2015-03-06 19:19:01
Although it feels a bit heavy, I want to make XY table either because it is new or the temperature is low but not two on each side, as one, remove it from the center to the end, and the other end aligns the height I will try it only for the wooden platform.
This review is about item#36291157.
I would like to make XY table on the drill by purchasing another short one.
4
From Japan
On 2015-03-06 09:17:53
I feel good because there is little wobble,
This review is about item#36291157.
Fastening the slide base
4
From Japan
On 2014-12-05 18:48:05
Although it was easy to use normally, I still do not know the durability.
This review is about item#36291157.
1
Customer Who Viewed This Item Also Viewed
Slide Rail S270
European Slide Rails
Slide Rail 17 New Series
Slide Rail
Double Step Slide Rails
Slide Rail
Slide Rail S101
Accuride: Slide Rail