Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Flexible Pipe

Flexible Pipe
Sales Price: 6.99 SGD
Review Rating: 4.25
4 Customer Reviews
5 star 1
4 star 3
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
External construction work
4
From Japan
On 2016-07-30 11:52:42
Because the degree of flexibility was as expected, it was possible to use without problems.
This review is about item#36568594.
Used as wiring cover of the power cable in the garage
5
From Japan
On 2014-08-16 10:48:52
I planned to install the power cable naked in the garage, but when I used this product, I was able to pay smartly.
This review is about item#36568594.
Air conditioner installation
4
From Japan
On 2014-03-02 00:18:38
I tried it indoors but it was nice and quite good. It felt a bit tight with the drain pipe and cable in 2 minutes and 3 minutes. It would be nice if there was a variation of color (bright cream color) and a size of size. (I think that we can use a lot in the indoor and outdoors.) Moreover, although I want a little more flexibility, I am satisfied with the price.
This review is about item#36568594.
Plumbing protection
4
From Japan
On 2013-09-20 13:23:51
I think that it is good if there are a number of bundles.
This review is about item#36568594.
1
Customer Who Viewed This Item Also Viewed
Duct
Flexible Air Duct
Slim Duct LD
Quick Duct 67Size
Mini Wall
Plug Cap
Free Corner, Flexi
Flexible
Free joint L 60-inch
Free joint L 80-inch
Indoor Slim Duct
Terminal Covering
Body Wall
Elbow, 90° Flat
Free joint (R Series)
Raceway End Cap
Free joint