Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Tire, "ML"

Tire, "ML"
Sales Price: 57.99 SGD
Review Rating: 4.90
10 Customer Reviews
5 star 9
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Vehicle maintenance
5
From Japan
On 2018-02-14 18:14:46
Cost performance is too good, after all Bridgestone.
This review is about item#36640983.
Tire change of a scooter
4
From Japan
On 2016-12-01 14:01:46
I bought it as a replacement rear tire for fusion. Although it decreased by about 6,000 km, it decreased considerably, but there are still more grooves near the center. It is recommended for those who place importance on town riding and COSPa.
This review is about item#36640807.
Used as a scooter rear wheel for newspaper delivery
5
From Japan
On 2016-10-24 19:23:48
Select a tire that you can use with confidence for use every morning. Although it is the same size with imported tires, I think cost performance is very high.
This review is about item#36641001.
To regular duties
5
From Japan
On 2015-06-24 21:23:41
There is no problem in particular.
This review is about item#36640721.
Tire recombination work
5
From Japan
On 2015-04-16 11:12:41
Very cheap, kind and polite correspondence, we are satisfied.
This review is about item#36640974.
Motorcycle maintenance
5
From Japan
On 2015-04-09 11:07:30
The price is reasonable and the delivery date is sure. Sincerely.
This review is about item#36640791.
Replace mini bike tires
5
From Japan
On 2014-07-25 10:09:54
I exchanged a tire of a mini bike. I was in embarrassment because the size of this hand was not so much else, but I feel satisfied that the inventory seems to be many and the delivery is also done quickly. I would like to also use it again.
This review is about item#36640721.
Tire exchange
5
From Japan
On 2013-06-17 04:43:51
Sidewalls are solid, there is moderate hardness and weight, there is security. Because the shape change is small during running, it can run steadily. Also, because it is not a fashionable trendy design, the balance of car body size and car weight etc of the original scooter is well taken and its goodness is manifested in the running. Blurring of the handle is lost, straight running stability improves. Because it is a front-only tire, the rudder becomes very easy to cut. Furthermore, it seems to be able to withstand use with a considerably high pneumatic pressure, and it seems that it can also be used for heavyweight car models. Although it was a replacement from a cheap tire of a certain D company, the difference in quality is showing up firmly at the price. Even if it is intended for use as a moped scooter, I think that it is a highly recommended tire to those who think that if you can buy peace of mind with money.
This review is about item#36640913.
Used in Honda MF 01 (Space 250)
5
From Japan
On 2013-04-27 14:01:04
I am on the old first freeway (MF 01) and the second generation freeway (MF 03). Initially the tire used Dunlop, but unexpectedly decreasing is early, so if it is this even cheaper one or the like, AUTOWAY scooter tire INNOVA (Inaver) which can be purchased for 2,500 yen is 120 / 90/10 in size of 1,980 It is about 2,780 yen from the yen and roughly half the price so it will decrease somewhat earlier but if I change over and over again I think that the cost per mileage will be much cheaper than the Bridgestone tires Though I bought it about 3 times and tried it down Is wearing at more than three times faster, the sidewall is also poor steering stability and the same size Bridgestone has 10,000 km but this has only about 1/3, before certainly going to 4,000 km The wire mesh will be exposed and it will not run. I tried three kinds of tires of AUTOWAY in the same size, but eventually they are together as a conclusion "the loss of money buying", not going to cheap but going up high. So next time I bought a YIFENG TIRE which is slightly higher than the same price in the same Chinese store price 2,980 yen. This is different from the tire for the scooter of the autoway, although the sidewall of the tire was firm, but with respect to the reduction it is not far behind the Bridgestone, wearing what is called Shinko tire of about 4,000 km, then 3,285 yen Although I saw it, it runs about 5,500 km, the central groove disappears and it becomes the replacement time, 5,000 km does not have Dunlop more than the Shinko tire is a little, but the sidewall is well well possessed, if the Bridgestone If I can not buy it I thought it was the best choice for my next choice. However, Bridgestone ML to buy with Monotaro is a price that cuts 5,000 yen by including shipping cost, although it is only about 1,000 yen compared with other YIFENG (postage included 3,500 yen) and Shinko tire (postage included 3,700 yen), the tire I felt that I had the best purchase when I comprehensively considered as having over twice. I am not a Japanese-made believer, but after all the bike tire is Bridgestone. I will buy only Bridgestone in the future!
This review is about item#36640791.
For replacement
5
From Japan
On 2012-11-15 18:02:26
A tire within one month from manufacturing arrived. It was good not to be old things.
This review is about item#36641001.
1
Customer Who Viewed This Item Also Viewed
Scooter Tires
Scooter Mini Bike Tire
Tire,
HOOP2 B02
MB520 URBAN MASTER
Tire, RUNSCOOT D307
Tire,
MICHELIN Tire S1
Tire,
Tire SCOOT SMART
MB99 DUAL
Throttle Cable
SL26
Dunlop Bike Tire
Scooter Tire, Big Scooter Supported
Scooter Tires