Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Bright Headlight Bulb

Bright Headlight Bulb
Sales Price: 34.99 SGD
Review Rating: 4.71
7 Customer Reviews
5 star 5
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Replace valve
5
From Japan
On 2018-02-13 14:57:32
It can be installed without problems. I also would like to purchase
This review is about item#36654886.
I use it as a motorcycle headlight bulb.
5
From Japan
On 2017-09-09 13:13:17
I use it for an old off-road bike. This is the third one to buy this valve. If you use cheap Petimon, it will expire soon, but this valve has a very long lifetime so I bought it. Even now I noticed that it seems that it has been over a year, so I bought it in advance. I do not know the brightness. It is absolutely dark no matter which valve is used up to now. Current road bikes and other headlamps are as bright as cars.
This review is about item#36654886.
Little Cub
5
From Japan
On 2016-10-09 21:23:01
Although it is expensive, I liked it brightly for a halogen. There are no signs that it will expire two months and a half from the wearing. It is awesome if it is easier a little more!
This review is about item#36654886.
It got brighter than the original light. Just exchanging work was a little hard. It seems that because the length of the lamp is longer than genuine and the fit inside the light was bad. Just because the lights are on properly there is no problem.
4
From Japan
On 2016-06-01 18:12:36
It seems that the person who got the genuine length position gets better in the light.
This review is about item#36654886.
Turnip repair
4
From Japan
On 2015-11-27 08:34:02
It is bright. I think it's good.
This review is about item#36654877.
Running the motorcycle at night
5
From Japan
On 2013-11-22 14:11:30
Until now the headlight was dark in the YAMAHA - DT50, it was very difficult to drive at night, but the headlight became much brighter as the DAYTONA bright headlight bulb was replaced, and night driving was able to travel safely even now, I regret that I should have bought it earlier. I will also buy next.
This review is about item#36654886.
Replacing bulb on headlight
5
From Japan
On 2013-08-06 12:19:44
I bought "22516". Because the originally attached bulb was 5W darker than genuine, it did not make a proper comparison, but after replacing to 22516 it became brighter overwhelmingly. Compared to HID and car headlights, it feels dark, of course, but you can see that the light reflecting on the body of the car running in front and the light reflected on the show window are definitely getting stronger. Also, when you enter a dark alley with few lights, you can secure the necessary and sufficient field of vision. For those who are worried about the darkness of motorcycle headlights, I think that it can be recommended enough as one of the countermeasure items.
This review is about item#36654886.
1